This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看到SN65DSI83的上电时序的参考波形图,EN是当DSI DATA 处于LP-11状态时将引脚拉高。
我们的板子上EN引脚用了复位芯片,由于该芯片本身有200ms的延迟,导致在LP-11状态已经过了之后才去拉高,如下图所示。此时驱动会提示“failed to lock pll”,这个无法正常工作也是符合预期的。
于是,我们将EN引脚的复位芯片去掉,并且使EN引脚硬件上一上电始终拉高,也就是在LP-11状态前使能引脚就已经处于高电平,此时驱动正常加载,器件能够正常工作,屏幕正常显示
所以,想确认一下,EN引脚始终拉高的情况下是否也符合SN65DSI83初始化时序?
您好,
必须按照 SN65DSI83-Q1 数据表的table 2中所述的通电顺序进行操作。
The DSI CLK lane MUST be in HS and the DSI data lanes MUST be driven to LP11 while the device is in reset before the EN pin is asserted per the timing described in Table 2.
EN管脚内部集成了上拉电阻,所以您可以对地接一个电容实现无源复位电路: