LMK3000内置VCO锁相芯片使用中芯片温度很高(烫手,估计至少在80摄氏度以上),配置程序能够实现指定频率点的输出功能(即VCO的分频功能正常),但调整内外的滤波电路始终无法实现锁相功能,其CP输出脚始终在3.3V,个人判断是鉴相功能没有实现,请各位帮忙分析一下原因,是不是芯片坏了? 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LMK3000内置VCO锁相芯片使用中芯片温度很高(烫手,估计至少在80摄氏度以上),配置程序能够实现指定频率点的输出功能(即VCO的分频功能正常),但调整内外的滤波电路始终无法实现锁相功能,其CP输出脚始终在3.3V,个人判断是鉴相功能没有实现,请各位帮忙分析一下原因,是不是芯片坏了? 谢谢!
LMK03000的LD pin是一个多功能管脚,其中模式9 (N Divider Output/2),可以用来判断VCO输出给N分频器这条路径是否正常;模式11 (R Divider Output/2),可以用来判断参考时钟到R分频器这条路径是否正常。请使用示波器测试波形,正常的话,LD这时输出都应该是鉴相频率的一半。
LMK03000可以支持方波输入,但是必须交流耦合,幅度在0.2~1.6V 之间。如果幅度太大,需要电阻分压后,再输入给LMK03000。环路滤波器是如何配置的?请使用CLock Design Tool 仿真优化环路参数。软件可从以下页面下载:www.ti.com.cn/.../clockdesigntool
VM92AD是批次号,K03000I表示器件型号,没有问题。
1,请确认寄存器配置值是否正确
使用Codeloader软件可生成,软件下载 www.ti.com.cn/.../codeloader 。配置文件可以被保存为.mac文件,如需检查,请附上.mac。Clock Design Tool的存盘文件.sav也请一道附上。
2,请检查MCU写寄存器的时序是否符合规格书的要求,寄存器是否成功写入LMK03000。
时序请参考LMK03000规格书 “Serial Data Timing Diagram”。请注意每个寄存器写完后 CLKuWire, DATAuWire, LEuWire电平都要回到低,LEuWire管脚最后有一个高电平脉冲,其上升沿和下降沿都是需要的。
要确认是否成功写入寄存器,可以使用R14 配置PLL_MUX管脚,强制Logic High,然后强制Logic Low,看PLL_MUX管脚电平是否变化。