Part Number: TUSB7320
Other Parts Discussed in Thread: TUSB7340
Question:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB7320
Other Parts Discussed in Thread: TUSB7340
Question:
Hi,
So I think the error is between the TUSB7320 and USB Disk(USB3.0 or USB2.0).
It's known issue to have errors when transferring balk files for Linux system.
But I can not find the source code,could you tell me how to get the source code?
Please allow some time for us to check if we have any source code other than firmware on TI.com.
When I check the MAX_PORTS of Host Controller Structural Parameters 1,For the TUSB7320, this field is 04h to indicate that 4 ports are supported.But I think TUSB7320 is only support 2 ports.Could you tell me why?
Will get back to you ASAP.
Thanks
Hi Cherry Zhou
>>It's known issue to have errors when transferring balk files for Linux system.
>>Please allow some time for us to check if we have any source code other than firmware on TI.com.
Thanks and best regards
If you know,could you tell me when transfering big size file from which version of Linux kernel?
And the file size when transfering?
Linux kernel is V5.10 , you were transferring Video files from camera, but not sure what size of the file.
For 2nd question, We will update on Tuesday.
Hi,
For 2nd question, TUSB7320 is the same die of TUSB7340,justn different M&B. So the MAX_PORTS of Host Controller Structural Parameters is same for both devices. 04h mean real 4 ports. Either 4 USB3 ports or 4 USB2 ports.
Hi Cherry Zhou,
Thanks and best regards
Hi,
Do you have the method to resolve the problem?
Sorry, please check with linux community.
And please see the link below for more assistance on your issue:
Hi,
So does 04h mean 2 USB3 ports + 2 USB2 ports = 4 ports?
4 ports mean 4 physical ports from port1 to port4, not 2 USB3 ports and 2 USB2 ports.
So I think it does not violate the errata.Is it right?
I agree with you, port 3 and port 4 are not disabled, it's not violate the errata.
But I can not find the source code,could you tell me how to get the source code?I want to reference it.
We don't have source code to share.
Thanks.
Hi Cherry Zhou,
Thanks and best regards
→I have no experience about linux community.Could you give any url about TSUB7320 about linux community?
this is a good source:
https://linux-hardware.org/?id=pci:104c-8241-1849-8241
→I knew it and methioned your share message.I am sorry to question again.But how about to explain the datasheet below about TUSB7340.(8 ports are supported.)
you are right, 4 ports means 2 USb3 ports and 2 USB2 ports.
Could you privode it to me? Is it windows driver?---------------------------------------------------------------The TI-provided driver for this device will not attempt to access disabled ports,but it is important that custom xHCI drivers andxHCI-aware BIOS implementations also do not attempt to access disabled ports.--------------------------------------------------------------->>Q5:I will check if we have any source code other than firmware on TI.com.→If you some source code,please give it to me.
Unfortunately we don't have any source code that can share.