Hi, TI Team
请问FPD-LINK的带宽和频率关系是怎么样的,例如,DS90UB954-Q1 FPD-LINK以4Gbps传输数据时,FPD-LINK上的信号频率是多少呢?是怎么计算的?
工作在COAX模式时,FPD-LINK是单端信号还是差分信号,测量眼图时该用单端探头还是差分探头?
B.R.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, TI Team
请问FPD-LINK的带宽和频率关系是怎么样的,例如,DS90UB954-Q1 FPD-LINK以4Gbps传输数据时,FPD-LINK上的信号频率是多少呢?是怎么计算的?
工作在COAX模式时,FPD-LINK是单端信号还是差分信号,测量眼图时该用单端探头还是差分探头?
B.R.
您好,两个概念,一个是line rata,,一个是信号频率,Line rate 指的是 FPD-LINK 串行总线上的高速信号的速率。
所以您提到的4Gbps应该就是指的line rate,那么高速信号的频率就是line rate的一半,即2Ghz。
工作在coax模式时,FPD link是单端信号,SER端的DOUT-和DES端的RIN-通过0.1uF电容到地,如下应用。
测量眼图时,建议使用差分探头,如果测量单端信号的话,那么DOUT-和下面连接方式一样,,通过50ohm电阻到地。

Hi, Kailyn,一个周期传2bit数据,我理解同时需要CLK线和DATA线,COAX只有一根线,是怎么同时传输时钟和数据的?不是太理解。
或者有说明FPD-LINK传输原理的文档吗?