This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550: 原理图检查

Part Number: TCAN4550


请帮忙检查一下这个原理图是否正确,有什么需要修改的地方?谢谢!

TCAN4550原理图检查20231007.pdf

  • 您好,看了下您的电路。

    1.Vsup电压范围6~24V。电路中没看到接的电压多少,所以这里注意下,另外,电路中的供电电压只使用了一颗旁路电容。建议参考EVM user's guide中的电路。

    2. Vio的电压可以是3.3V或者5V。

    3.电路中很多部分都看不到,接在Soc端的,8 (nINT) 和 9 (GPO2) 是open drain输出,需要上拉电阻到Vio,上拉电阻范围可以是2Kohm~10Kohm范围。

    4. CAN和和CANL输出端的阻值R3,R4为60omh匹配电阻,C2 的值可以4700pF。

    5.晶振的负载电容我看使用的是22pF,结合晶振的Spec要符合晶振的负载电容。如果不能正常起振,可以参考下面这篇关于晶振选型以及设计要求的应用手册:

    https://www.ti.com.cn/cn/lit/an/slla549/slla549.pdf