This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,输出出现了overshoot,建议在输出端串联个小电阻再试试,比如100ohm电阻。
验证下波形是否改善? EVM 原理图串联的是0ohm阻值,您这边串联个100ohm的验证下。
您好,目前的问题不是overshoot,问题是DDC信号经过SN65DP159后的信号延时不同,导致了SDA和SCL的时序存在风险,部分主机无法读取显示器的EDID,需要在SDA_SNK线增加一个2.2nF的电容对地,才能正常读取EDID。规格书中只是说明SRC to SNK和SNK to SRC的信号会延时,但实际测量到的信号不仅仅会延时(实测延时值为40uS,比规格书的230nS大很多),同时DDC信号的时序也会被改变(SCL第一个低电平的时间被明显缩短了)。以下是DDC信号在DP159前后的实测波形:
1、进入DP159前的DDC信号,其中黄色为SCL_SRC,红色为SDA_SRC
2、经过DP159后的DDC信号,其中黄色为SCL_SNK,红色为SDA_SNK
可以明显看到SDA和SCL的延时不同,哪些原因可能会导致这个问题?
测试波形是在DP159端(TMDS181的DDC存在同样的问题)。
下图是DP159的部分电路,I2C部分电路上拉了2k电阻,左边是接FPGA,右边是接HDMI接口。
您好,I2C部分源端上拉2K没问题,sink端需要上拉47K。
这是DP159的原理图checklist:
https://www.ti.com.cn/cn/lit/an/slla461/slla461.pdf
另外您提到TMDS181也是这个问题,TMDS181 支持clock stretching。我想问下您这边应用HDMI端是否支持I2C clock stretching mode?