This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74TVC3010低电平被拉高

Other Parts Discussed in Thread: SN74TVC3010

你好,

请教两个问题,我用SN74TVC3010按照PDF的说明,在5V输出端接了一个150欧电阻,结果5V输入信号(方波信号)直接被拉成高电平;换成1K电阻,结果5V输入信号和3.3V输出信号的GND都被拉高了,GND在1V的位置上,好像信号的GND浮空一样。

请问怎样把输入输出信号的低电平拉低到正常位置?  

还有如果不加上拉电阻,怎么设计电路使3.3V输入 5V输出?

亟待回复,谢谢。

  • pull high 电阻关系到电流的驱动能力,即和电压的电流大小有关,

    依据您的情况请尝试将pull high电阻换为10K,

    不加上拉电阻?3.3V输入,5V输出...还是用SN74TVC3010吗?

  • 还是用SN74TVC3010,不加上拉电阻,能实现3.3V输入,5V输出吗?

  • 不加pull high怎么实现电平转换?

  • 还有一个问题,我用信号发生器输入方波信号,在5V输出端用示波器观察,5V端有上拉电阻,随着输入信号频率的上升,输出端的信号逐渐失真,表现是上升沿先有尖脉冲到6V,然后下降到4V,再逐渐上升到5V,此时要想得到标准的方波波形,只能更换不同阻值的上拉电阻才行,请问这是怎么回事?谢谢

  • 请问您是增大还是减小阻值呢?应该是减小吧~~~

    overshoot的产生有很多情况,您描述的在高频情况下产生应该算是正常,可以加电容试试

x 出现错误。请重试或与管理员联系。