Other Parts Discussed in Thread: TRS3227, , MAX3227
工程师你好,
目前我们需要一个可以防止RS232外部短路的232接口芯片(或电路),具体工况如下:
1.RS232-TX对GND短路时;
2.RS232-TX对VCC短路时;
3.RS232-RX对GND短路时;
4.RS232-RX对VCC短路时;
以上4种短路工况下,是否有现成的RS232收发芯片可以直接集成短路防护功能的?如果没有,请问针对以上4个短路工况,该如何处理呢?
感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我看了下我们的收发器,232的收发器有集成短路保护的,但是针对IO开路保护。其他的RS232器件比如MAX3227/TRS3227的ESD防护等级要比MAX232 好一些。
短路保护的收发器比如RS422或者RS485会有。
那对于RS232来说,如果需要对IO进行短路保护,可以考虑使用TVS。
我看在这个帖子里推荐的是Bourns 公司的TBU-CA系列保护器件。
您参考下: