Other Parts Discussed in Thread: TPS650061
TUSB9261 电脑无法识别 ,指示灯状态为:D6,长灭,其他指示灯长亮

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
WIN10系统,安装TUSB926x_Burner软件过程中没有弹出需要安装驱动的界面
您好,您看下这个帖子,在安装TUSB926x_Burner时是不是遇到的问题一样?
我看E2E发给他对应的文件,您看下您是否方便在E2E上咨询这个问题,然后随时跟进?如果不方便,我这边帮您提交到E2E也可以的。
您好,感谢您的反馈,通常来说不能识别到硬盘的原因是因为SATA接口的极性问题。
TUSB9261的firmware文件夹中包含了TX,RX极性 相反,以及极性没有相反的固件,您要看下实际layout中有没有极性相反,然后确定使用哪一个固件程序。
TUSB9261 demo中默认的是TX的极性相反。
这几个耦合电容不会影响。
需要注意的是差分线要尽量走的等长等间距,最好长度差保持在2.5mil之内。
另外就是100ohm的特征阻抗。
我怀疑是SPI的问题,您量SPI时序了没?
另外就是需要注意上电时序,参考7.3.1.4 Power-Up and Reset Sequence。GRST引脚您是怎么接的?
电源时序没问题。所以不是这里的问题。
另外我的EEPROM用的是M95512-RMN6TP,不知道有没有影响
demo中使用的是Pm25LV512A.。
datasheet 8.2.2.4中给出了flash的一些要求,可以看下。但我认为满足这些条件的替换为其他flash型号应该也是可以的。

另外,我看TUSB9261的指南手册中推荐了SPI flash的几款经过验证的型号:

关于TUSB9261 SPI flash的要求,总结下来以下几点:
满足下面要求的应该都是可以的。另外,TUSB9261 支持SPI mode0, 不支持SPI mode1.
~ The bootloader uses a fixed frequency of 18.75 MHz, flash should support this clock frequency.
~ The flash must use a word size of 8 bits and an address length of 24 bits.
~ The program instruction must allow 256 bytes to be written in one operation.
~ The entire chip should be able to be erased by the bootloader prior to programming.
~ Minimum flash size of 512 kbits (64 k x 8).