This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1043-Q1: INH状态

Part Number: TCAN1043-Q1

各位TI的专家好,

我在使用TCAN1043时遇到一个问题,我们的产品使用了INH功能来控制一级DCDC的使能,

在做从0V到12V的上升实验时,步进为0.5V/min,产品无法正常启动,测量1043的几个管脚电压,

INH:11.8V,EN/STB/VIO/VCC,0V,这个状态下INH还是高,是正常状态吗?

谢谢。