This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS80PCI402寄存器配置不起作用问题

Other Parts Discussed in Thread: DS80PCI402

我们在pcie1.0上面应用DS80PCI402做repeater功能,现在存在的问题是,iic寄存器能够正常写入,读出的值与写入的值均正确,但是从测试的信号上看,该寄存器该起的作用根本没有起作用:

1、尤其比较明显的0x01中,disable所有的channel,这时测试输出引脚仍然有信号输出;

2、请帮忙确认下,在2.5V供电是,VIN和VDD_SEL引脚的电平值为 2.5V是否正确,原则上应该是悬空,在后面解释float时,说的是2/3VDD,但是我实际测试出来就是2.5V;

3、寄存器中,0x00中的第0位,是软件的reset恢复所有寄存器为default设置状态,但是实际测试时,发现改位设置也是不管用,原来的寄存器设置值仍然会保持。

请各位大师帮下忙