我用DS90C385AMT做的线路板,后来发现这颗料温度特性不是很好,想找个能适用于低温的,找到SN65LVDS93ADGG,想在不改动PCB的情况下,之替换IC,不知这样可行?看手册,这两颗料的管脚定义都一样,封装也一样
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用DS90C385AMT做的线路板,后来发现这颗料温度特性不是很好,想找个能适用于低温的,找到SN65LVDS93ADGG,想在不改动PCB的情况下,之替换IC,不知这样可行?看手册,这两颗料的管脚定义都一样,封装也一样
二者的引脚和封装都一样,相比之下,SN65LVDS93A的性能要比DS90C385要好一些,SN65LVDS93A的PLL频率范围为10~135MHz,而DS90C385的频率范围为18~87.5Mhz,SN65LVDS93A能工作在1.8V的低压下,1.8~3.3V范围,而DS90C385只能3.3V。 或者可参考下DS90CR285,引脚和封装也相同,温度范围也-40~85度。
你好,目前我们的打算使用SN65LVDS93A作为并转串的芯片,但是发现93A配套的解串器,SN65LVDS94他的PCLK直到68Mhz,而93A 可以到135Mhz,
所以想咨询下,能够给93A配对解串的,PCLK频率更高的芯片有哪个? 我自己找了下,DS90CF386和ds90cr288a貌似可以,但是不太确定。希望能帮助解答,谢谢啦。
SN65LVDS93A是SN65LVDS93的升级版本,所以PLL的频率也升级到了135MHz,以前SN65LVDS93和SN65LVDS94是配对的,都是最高68Mhz的。
DS90CF386和ds90cr288a的PCLK最高是85MHz,如果你的应用中PCLK的频率不超过68MHz的话,还是建议采用SN65LVDS94来解串。
你好,请问SN65LVDS93A数据编码后,是否可用DS90CR288作为解码芯片?谢谢
可以,配置为但是SN65LVDS93A的最高像素时钟达135Mhz,而DS90CR288最高85Mhz,所以使用DS90CR288解码的话,像素时钟控制在85Mhz。