Part Number: DP83867IS
Hi Ti experts,
My schematic is as follow。The PC cannot find the PHY when power on the circuit。

I do the following try:
1.Add the divider capacitor in XI pin as follows,the value of CD1 and CD2 is 27 pF.

2.Remove resistor R238 and R240;change the value of R235 to10 kΩ,and change the value of R236 to 2.49kΩ;let one pin of R236 connect to net ETHA_LED0 and another to
.


3.Change the RJ45 to the next circuit and connect
with
by a capacitor of 4.7nF