This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947-Q1: DS90UB947与DS90UB688是否可以匹配使用?

Part Number: DS90UB947-Q1


DS90UB947(主控制器#1)与DS90UB948/928(显示总成#1)搭配使用,FPD LINK III,Dual Link,显示和通信控制均正常;

我司产品解串器需要切换成DS90UB688,这个视频流协议改成了FPD LINK IV,请问 DS90UB947(主控制器#1)与DS90UB688(显示总成#1)是否可以继续搭配使用?

另关于947、948、928、688芯片,我司与TI原厂已经签过NDA文件,谢谢

  • 您好,DS90UB688可以向下兼容,和DS90UB947搭配使用。

    有寄存器是可以配置输入是FPD3还是FPD4。

    已经签署过NDA协议的话,可以继续申请DS90UB688的数据手册参考下。

  • 谢谢你的回复!

    我们还有如下疑问:

    1,我们使用FPD4的串行器(DS90Ux943A)主机(主控制器#1)匹配DS90UB688的产品(显示总成#1),协议为FPD4;

    2,同时我们还需要使用FPD3的串行器(DS90UB947)主机(主控制器#2)匹配DS90UB688(显示总成#1),协议为FPD3;

    请问以上方案是否可行?谢谢!

    再帮忙确认如下理解是否正确?

    由于 显示总成#1 设置了FPD4,当 显示总成#1 再去匹配 主控制器#2 的时候,由于 主控制器#2 仅支持FPD3,所以 主控制器#2 无法Link Lock 显示总成#1,无法通过IIC访问,无法通过寄存器更改 显示总成#1 协议为FPD3!我的理解对吗?

    谢谢!

  • 我们使用FPD4的串行器(DS90Ux943A)主机(主控制器#1)匹配DS90UB688的产品(显示总成#1),协议为FPD4;

    您的意思是要确认943是否可以和688搭配使用吗?----可以的。

    同时我们还需要使用FPD3的串行器(DS90UB947)主机(主控制器#2)匹配DS90UB688(显示总成#1),协议为FPD3;

    947也可以和688搭配使用。

    还是说上述两个条件是一个方案?能否将方案框图附上?