Part Number: TCAN4550
有没有安卓平台的驱动,目前的代码差异比较大,需要安卓平台的驱动
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,关于TCAN4550 驱动的帖子很多,包括您说的linux或者C:
但是没有找到关于安卓的驱动。
关于上掉电时序,建议参考datasheet Figure 15-18的时序图,包括上电时序,normal to sleep 或者sleep to standby的时序要求。
硬件上如果有什么问题,我们可一起讨论。
安卓的驱动能不能参考其他家的IC代码修改一下,只改寄存器相关的内容?我这边自己写太耗时间了,因为对IC的寄存器配置部分也不太熟悉。需要原厂处理IC的部分,我这边只处理平台部分.下面发的驱动也是安卓自带别家的IC的驱动,也是SPI的.
/* CAN bus driver for Holt HI3110 CAN Controller with SPI Interface
*
* Copyright(C) Timesys Corporation 2016
*
* Based on Microchip 251x CAN Controller (mcp251x) Linux kernel driver
* Copyright 2009 Christian Pellegrin EVOL S.r.l.
* Copyright 2007 Raymarine UK, Ltd. All Rights Reserved.
* Copyright 2006 Arcom Control Systems Ltd.
*
* Based on CAN bus driver for the CCAN controller written by
* - Sascha Hauer, Marc Kleine-Budde, Pengutronix
* - Simon Kallweit, intefo AG
* Copyright 2007
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
#include <linux/can/core.h>
#include <linux/can/dev.h>
#include <linux/can/led.h>
#include <linux/clk.h>
#include <linux/completion.h>
#include <linux/delay.h>
#include <linux/device.h>
#include <linux/dma-mapping.h>
#include <linux/freezer.h>
#include <linux/interrupt.h>
#include <linux/io.h>
#include <linux/kernel.h>
#include <linux/module.h>
#include <linux/netdevice.h>
#include <linux/of.h>
#include <linux/of_device.h>
#include <linux/platform_device.h>
#include <linux/regulator/consumer.h>
#include <linux/slab.h>
#include <linux/spi/spi.h>
#include <linux/uaccess.h>
#define HI3110_MASTER_RESET 0x56
#define HI3110_READ_CTRL0 0xD2
#define HI3110_READ_CTRL1 0xD4
#define HI3110_READ_STATF 0xE2
#define HI3110_WRITE_CTRL0 0x14
#define HI3110_WRITE_CTRL1 0x16
#define HI3110_WRITE_INTE 0x1C
#define HI3110_WRITE_BTR0 0x18
#define HI3110_WRITE_BTR1 0x1A
#define HI3110_READ_BTR0 0xD6
#define HI3110_READ_BTR1 0xD8
#define HI3110_READ_INTF 0xDE
#define HI3110_READ_ERR 0xDC
#define HI3110_READ_FIFO_WOTIME 0x48
#define HI3110_WRITE_FIFO 0x12
#define HI3110_READ_MESSTAT 0xDA
#define HI3110_READ_REC 0xEA
#define HI3110_READ_TEC 0xEC
#define HI3110_CTRL0_MODE_MASK (7 << 5)
#define HI3110_CTRL0_NORMAL_MODE (0 << 5)
#define HI3110_CTRL0_LOOPBACK_MODE (1 << 5)
#define HI3110_CTRL0_MONITOR_MODE (2 << 5)
#define HI3110_CTRL0_SLEEP_MODE (3 << 5)
#define HI3110_CTRL0_INIT_MODE (4 << 5)
#define HI3110_CTRL1_TXEN BIT(7)
#define HI3110_INT_RXTMP BIT(7)
#define HI3110_INT_RXFIFO BIT(6)
#define HI3110_INT_TXCPLT BIT(5)
#define HI3110_INT_BUSERR BIT(4)
#define HI3110_INT_MCHG BIT(3)
#define HI3110_INT_WAKEUP BIT(2)
#define HI3110_INT_F1MESS BIT(1)
#define HI3110_INT_F0MESS BIT(0)
#define HI3110_ERR_BUSOFF BIT(7)
#define HI3110_ERR_TXERRP BIT(6)
#define HI3110_ERR_RXERRP BIT(5)
#define HI3110_ERR_BITERR BIT(4)
#define HI3110_ERR_FRMERR BIT(3)
#define HI3110_ERR_CRCERR BIT(2)
#define HI3110_ERR_ACKERR BIT(1)
#define HI3110_ERR_STUFERR BIT(0)
#define HI3110_ERR_PROTOCOL_MASK (0x1F)
#define HI3110_ERR_PASSIVE_MASK (0x60)
#define HI3110_STAT_RXFMTY BIT(1)
#define HI3110_STAT_BUSOFF BIT(2)
#define HI3110_STAT_ERRP BIT(3)
#define HI3110_STAT_ERRW BIT(4)
#define HI3110_STAT_TXMTY BIT(7)
#define HI3110_BTR0_SJW_SHIFT 6
#define HI3110_BTR0_BRP_SHIFT 0
#define HI3110_BTR1_SAMP_3PERBIT (1 << 7)
#define HI3110_BTR1_SAMP_1PERBIT (0 << 7)
#define HI3110_BTR1_TSEG2_SHIFT 4
#define HI3110_BTR1_TSEG1_SHIFT 0
#define HI3110_FIFO_WOTIME_TAG_OFF 0
#define HI3110_FIFO_WOTIME_ID_OFF 1
#define HI3110_FIFO_WOTIME_DLC_OFF 5
#define HI3110_FIFO_WOTIME_DAT_OFF 6
#define HI3110_FIFO_WOTIME_TAG_IDE BIT(7)
#define HI3110_FIFO_WOTIME_ID_RTR BIT(0)
#define HI3110_FIFO_TAG_OFF 0
#define HI3110_FIFO_ID_OFF 1
#define HI3110_FIFO_STD_DLC_OFF 3
#define HI3110_FIFO_STD_DATA_OFF 4
#define HI3110_FIFO_EXT_DLC_OFF 5
#define HI3110_FIFO_EXT_DATA_OFF 6
#define HI3110_CAN_MAX_DATA_LEN 8
#define HI3110_RX_BUF_LEN 15
#define HI3110_TX_STD_BUF_LEN 12
#define HI3110_TX_EXT_BUF_LEN 14
#define HI3110_CAN_FRAME_MAX_BITS 128
#define HI3110_EFF_FLAGS 0x18 /* IDE + SRR */
#define HI3110_TX_ECHO_SKB_MAX 1
#define HI3110_OST_DELAY_MS (10)
#define DEVICE_NAME "hi3110"
static int hi3110_enable_dma = 1; /* Enable SPI DMA. Default: 1 (On) */
module_param(hi3110_enable_dma, int, 0444);
MODULE_PARM_DESC(hi3110_enable_dma, "Enable SPI DMA. Default: 1 (On)");
static const struct can_bittiming_const hi3110_bittiming_const = {
.name = DEVICE_NAME,
.tseg1_min = 2,
.tseg1_max = 16,
.tseg2_min = 2,
.tseg2_max = 8,
.sjw_max = 4,
.brp_min = 1,
.brp_max = 64,
.brp_inc = 1,
};
enum hi3110_model {
CAN_HI3110_HI3110 = 0x3110,
};
struct hi3110_priv {
struct can_priv can;
struct net_device *net;
struct spi_device *spi;
enum hi3110_model model;
struct mutex hi3110_lock; /* SPI device lock */
u8 *spi_tx_buf;
u8 *spi_rx_buf;
dma_addr_t spi_tx_dma;
dma_addr_t spi_rx_dma;
struct sk_buff *tx_skb;
int tx_len;
struct workqueue_struct *wq;
struct work_struct tx_work;
struct work_struct restart_work;
int force_quit;
int after_suspend;
#define HI3110_AFTER_SUSPEND_UP 1
#define HI3110_AFTER_SUSPEND_DOWN 2
#define HI3110_AFTER_SUSPEND_POWER 4
#define HI3110_AFTER_SUSPEND_RESTART 8
int restart_tx;
struct regulator *power;
struct regulator *transceiver;
struct clk *clk;
};
static void hi3110_clean(struct net_device *net)
{
struct hi3110_priv *priv = netdev_priv(net);
if (priv->tx_skb || priv->tx_len)
net->stats.tx_errors++;
if (priv->tx_skb)
dev_kfree_skb(priv->tx_skb);
if (priv->tx_len)
can_free_echo_skb(priv->net, 0);
priv->tx_skb = NULL;
priv->tx_len = 0;
}
/* Note about handling of error return of hi3110_spi_trans: accessing
* registers via SPI is not really different conceptually than using
* normal I/O assembler instructions, although it's much more
* complicated from a practical POV. So it's not advisable to always
* check the return value of this function. Imagine that every
* read{b,l}, write{b,l} and friends would be bracketed in "if ( < 0)
* error();", it would be a great mess (well there are some situation
* when exception handling C++ like could be useful after all). So we
* just check that transfers are OK at the beginning of our
* conversation with the chip and to avoid doing really nasty things
* (like injecting bogus packets in the network stack).
*/
static int hi3110_spi_trans(struct spi_device *spi, int len)
{
struct hi3110_priv *priv = spi_get_drvdata(spi);
struct spi_transfer t = {
.tx_buf = priv->spi_tx_buf,
.rx_buf = priv->spi_rx_buf,
.len = len,
.cs_change = 0,
};
struct spi_message m;
int ret;
spi_message_init(&m);
if (hi3110_enable_dma) {
t.tx_dma = priv->spi_tx_dma;
t.rx_dma = priv->spi_rx_dma;
m.is_dma_mapped = 1;
}
spi_message_add_tail(&t, &m);
ret = spi_sync(spi, &m);
if (ret)
dev_err(&spi->dev, "spi transfer failed: ret = %d\n", ret);
return ret;
}
static u8 hi3110_cmd(struct spi_device *spi, u8 command)
{
struct hi3110_priv *priv = spi_get_drvdata(spi);
priv->spi_tx_buf[0] = command;
dev_dbg(&spi->dev, "hi3110_cmd: %02X\n", command);
return hi3110_spi_trans(spi, 1);
}
static u8 hi3110_read(struct spi_device *spi, u8 command)
{
struct hi3110_priv *priv = spi_get_drvdata(spi);
u8 val = 0;
priv->spi_tx_buf[0] = command;
hi3110_spi_trans(spi, 2);
val = priv->spi_rx_buf[1];
return val;
}
static void hi3110_write(struct spi_device *spi, u8 reg, u8 val)
{
struct hi3110_priv *priv = spi_get_drvdata(spi);
priv->spi_tx_buf[0] = reg;
priv->spi_tx_buf[1] = val;
hi3110_spi_trans(spi, 2);
}
static void hi3110_hw_tx_frame(struct spi_device *spi, u8 *buf, int len)
{
struct hi3110_priv *priv = spi_get_drvdata(spi);
priv->spi_tx_buf[0] = HI3110_WRITE_FIFO;
memcpy(priv->spi_tx_buf + 1, buf, len);
hi3110_spi_trans(spi, len + 1);
}
static void hi3110_hw_tx(struct spi_device *spi, struct can_frame *frame)
{
u8 buf[HI3110_TX_EXT_BUF_LEN];
buf[HI3110_FIFO_TAG_OFF] = 0;
if (frame->can_id & CAN_EFF_FLAG) {
/* Extended frame */
buf[HI3110_FIFO_ID_OFF] = (frame->can_id & CAN_EFF_MASK) >> 21;
buf[HI3110_FIFO_ID_OFF + 1] =
(((frame->can_id & CAN_EFF_MASK) >> 13) & 0xe0) |
HI3110_EFF_FLAGS |
(((frame->can_id & CAN_EFF_MASK) >> 15) & 0x07);
buf[HI3110_FIFO_ID_OFF + 2] =
(frame->can_id & CAN_EFF_MASK) >> 7;
buf[HI3110_FIFO_ID_OFF + 3] =
((frame->can_id & CAN_EFF_MASK) << 1) |
((frame->can_id & CAN_RTR_FLAG) ? 1 : 0);
buf[HI3110_FIFO_EXT_DLC_OFF] = frame->can_dlc;
memcpy(buf + HI3110_FIFO_EXT_DATA_OFF,
frame->data, frame->can_dlc);
hi3110_hw_tx_frame(spi, buf, HI3110_TX_EXT_BUF_LEN -
(HI3110_CAN_MAX_DATA_LEN - frame->can_dlc));
} else {
/* Standard frame */
buf[HI3110_FIFO_ID_OFF] = (frame->can_id & CAN_SFF_MASK) >> 3;
buf[HI3110_FIFO_ID_OFF + 1] =
((frame->can_id & CAN_SFF_MASK) << 5) |
((frame->can_id & CAN_RTR_FLAG) ? (1 << 4) : 0);
buf[HI3110_FIFO_STD_DLC_OFF] = frame->can_dlc;
memcpy(buf + HI3110_FIFO_STD_DATA_OFF,
frame->data, frame->can_dlc);
hi3110_hw_tx_frame(spi, buf, HI3110_TX_STD_BUF_LEN -
(HI3110_CAN_MAX_DATA_LEN - frame->can_dlc));
}
}
static void hi3110_hw_rx_frame(struct spi_device *spi, u8 *buf)
{
struct hi3110_priv *priv = spi_get_drvdata(spi);
priv->spi_tx_buf[0] = HI3110_READ_FIFO_WOTIME;
hi3110_spi_trans(spi, HI3110_RX_BUF_LEN);
memcpy(buf, priv->spi_rx_buf + 1, HI3110_RX_BUF_LEN - 1);
}
static void hi3110_hw_rx(struct spi_device *spi)
{
struct hi3110_priv *priv = spi_get_drvdata(spi);
struct sk_buff *skb;
struct can_frame *frame;
u8 buf[HI3110_RX_BUF_LEN - 1];
skb = alloc_can_skb(priv->net, &frame);
if (!skb) {
priv->net->stats.rx_dropped++;
return;
}
hi3110_hw_rx_frame(spi, buf);
if (buf[HI3110_FIFO_WOTIME_TAG_OFF] & HI3110_FIFO_WOTIME_TAG_IDE) {
/* IDE is recessive (1), indicating extended 29-bit frame */
frame->can_id = CAN_EFF_FLAG;
frame->can_id |=
(buf[HI3110_FIFO_WOTIME_ID_OFF] << 21) |
(((buf[HI3110_FIFO_WOTIME_ID_OFF + 1] & 0xE0) >> 5) << 18) |
((buf[HI3110_FIFO_WOTIME_ID_OFF + 1] & 0x07) << 15) |
(buf[HI3110_FIFO_WOTIME_ID_OFF + 2] << 7) |
(buf[HI3110_FIFO_WOTIME_ID_OFF + 3] >> 1);
} else {
/* IDE is dominant (0), frame indicating standard 11-bit */
frame->can_id =
(buf[HI3110_FIFO_WOTIME_ID_OFF] << 3) |
((buf[HI3110_FIFO_WOTIME_ID_OFF + 1] & 0xE0) >> 5);
}
/* Data length */
frame->can_dlc = get_can_dlc(buf[HI3110_FIFO_WOTIME_DLC_OFF] & 0x0F);
if (buf[HI3110_FIFO_WOTIME_ID_OFF + 3] & HI3110_FIFO_WOTIME_ID_RTR)
frame->can_id |= CAN_RTR_FLAG;
else
memcpy(frame->data, buf + HI3110_FIFO_WOTIME_DAT_OFF,
frame->can_dlc);
priv->net->stats.rx_packets++;
priv->net->stats.rx_bytes += frame->can_dlc;
can_led_event(priv->net, CAN_LED_EVENT_RX);
netif_rx_ni(skb);
}
static void hi3110_hw_sleep(struct spi_device *spi)
{
hi3110_write(spi, HI3110_WRITE_CTRL0, HI3110_CTRL0_SLEEP_MODE);
}
static netdev_tx_t hi3110_hard_start_xmit(struct sk_buff *skb,
struct net_device *net)
{
struct hi3110_priv *priv = netdev_priv(net);
struct spi_device *spi = priv->spi;
if (priv->tx_skb || priv->tx_len) {
dev_err(&spi->dev, "hard_xmit called while tx busy\n");
return NETDEV_TX_BUSY;
}
if (can_dropped_invalid_skb(net, skb))
return NETDEV_TX_OK;
netif_stop_queue(net);
priv->tx_skb = skb;
queue_work(priv->wq, &priv->tx_work);
return NETDEV_TX_OK;
}
static int hi3110_do_set_mode(struct net_device *net, enum can_mode mode)
{
struct hi3110_priv *priv = netdev_priv(net);
switch (mode) {
case CAN_MODE_START:
hi3110_clean(net);
/* We have to delay work since SPI I/O may sleep */
priv->can.state = CAN_STATE_ERROR_ACTIVE;
priv->restart_tx = 1;
if (priv->can.restart_ms == 0)
priv->after_suspend = HI3110_AFTER_SUSPEND_RESTART;
queue_work(priv->wq, &priv->restart_work);
break;
default:
return -EOPNOTSUPP;
}
return 0;
}
static int hi3110_get_berr_counter(const struct net_device *net,
struct can_berr_counter *bec)
{
struct hi3110_priv *priv = netdev_priv(net);
struct spi_device *spi = priv->spi;
mutex_lock(&priv->hi3110_lock);
bec->txerr = hi3110_read(spi, HI3110_READ_TEC);
bec->rxerr = hi3110_read(spi, HI3110_READ_REC);
mutex_unlock(&priv->hi3110_lock);
return 0;
}
static int hi3110_set_normal_mode(struct spi_device *spi)
{
struct hi3110_priv *priv = spi_get_drvdata(spi);
u8 reg = 0;
hi3110_write(spi, HI3110_WRITE_INTE, HI3110_INT_BUSERR |
HI3110_INT_RXFIFO | HI3110_INT_TXCPLT);
/* Enable TX */
hi3110_write(spi, HI3110_WRITE_CTRL1, HI3110_CTRL1_TXEN);
if (priv->can.ctrlmode & CAN_CTRLMODE_LOOPBACK)
reg = HI3110_CTRL0_LOOPBACK_MODE;
else if (priv->can.ctrlmode & CAN_CTRLMODE_LISTENONLY)
reg = HI3110_CTRL0_MONITOR_MODE;
else
reg = HI3110_CTRL0_NORMAL_MODE;
hi3110_write(spi, HI3110_WRITE_CTRL0, reg);
/* Wait for the device to enter the mode */
mdelay(HI3110_OST_DELAY_MS);
reg = hi3110_read(spi, HI3110_READ_CTRL0);
if ((reg & HI3110_CTRL0_MODE_MASK) != reg)
return -EBUSY;
priv->can.state = CAN_STATE_ERROR_ACTIVE;
return 0;
}
static int hi3110_do_set_bittiming(struct net_device *net)
{
struct hi3110_priv *priv = netdev_priv(net);
struct can_bittiming *bt = &priv->can.bittiming;
struct spi_device *spi = priv->spi;
hi3110_write(spi, HI3110_WRITE_BTR0,
((bt->sjw - 1) << HI3110_BTR0_SJW_SHIFT) |
((bt->brp - 1) << HI3110_BTR0_BRP_SHIFT));
hi3110_write(spi, HI3110_WRITE_BTR1,
(priv->can.ctrlmode &
CAN_CTRLMODE_3_SAMPLES ?
HI3110_BTR1_SAMP_3PERBIT : HI3110_BTR1_SAMP_1PERBIT) |
((bt->phase_seg1 + bt->prop_seg - 1)
<< HI3110_BTR1_TSEG1_SHIFT) |
((bt->phase_seg2 - 1) << HI3110_BTR1_TSEG2_SHIFT));
dev_dbg(&spi->dev, "BT: 0x%02x 0x%02x\n",
hi3110_read(spi, HI3110_READ_BTR0),
hi3110_read(spi, HI3110_READ_BTR1));
return 0;
}
static int hi3110_setup(struct net_device *net)
{
hi3110_do_set_bittiming(net);
return 0;
}
static int hi3110_hw_reset(struct spi_device *spi)
{
u8 reg;
int ret;
/* Wait for oscillator startup timer after power up */
mdelay(HI3110_OST_DELAY_MS);
ret = hi3110_cmd(spi, HI3110_MASTER_RESET);
if (ret)
return ret;
/* Wait for oscillator startup timer after reset */
mdelay(HI3110_OST_DELAY_MS);
reg = hi3110_read(spi, HI3110_READ_CTRL0);
if ((reg & HI3110_CTRL0_MODE_MASK) != HI3110_CTRL0_INIT_MODE)
return -ENODEV;
/* As per the datasheet it appears the error flags are
* not cleared on reset. Explicitly clear them by performing a read
*/
hi3110_read(spi, HI3110_READ_ERR);
return 0;
}
static int hi3110_hw_probe(struct spi_device *spi)
{
u8 statf;
hi3110_hw_reset(spi);
/* Confirm correct operation by checking against reset values
* in datasheet
*/
statf = hi3110_read(spi, HI3110_READ_STATF);
dev_dbg(&spi->dev, "statf: %02X\n", statf);
if (statf != 0x82)
return -ENODEV;
return 0;
}
static int hi3110_power_enable(struct regulator *reg, int enable)
{
if (IS_ERR_OR_NULL(reg))
return 0;
if (enable)
return regulator_enable(reg);
else
return regulator_disable(reg);
}
static int hi3110_stop(struct net_device *net)
{
struct hi3110_priv *priv = netdev_priv(net);
struct spi_device *spi = priv->spi;
close_candev(net);
priv->force_quit = 1;
free_irq(spi->irq, priv);
destroy_workqueue(priv->wq);
priv->wq = NULL;
mutex_lock(&priv->hi3110_lock);
/* Disable transmit, interrupts and clear flags */
hi3110_write(spi, HI3110_WRITE_CTRL1, 0x0);
hi3110_write(spi, HI3110_WRITE_INTE, 0x0);
hi3110_read(spi, HI3110_READ_INTF);
hi3110_clean(net);
hi3110_hw_sleep(spi);
hi3110_power_enable(priv->transceiver, 0);
priv->can.state = CAN_STATE_STOPPED;
mutex_unlock(&priv->hi3110_lock);
can_led_event(net, CAN_LED_EVENT_STOP);
return 0;
}
static void hi3110_tx_work_handler(struct work_struct *ws)
{
struct hi3110_priv *priv = container_of(ws, struct hi3110_priv,
tx_work);
struct spi_device *spi = priv->spi;
struct net_device *net = priv->net;
struct can_frame *frame;
mutex_lock(&priv->hi3110_lock);
if (priv->tx_skb) {
if (priv->can.state == CAN_STATE_BUS_OFF) {
hi3110_clean(net);
} else {
frame = (struct can_frame *)priv->tx_skb->data;
hi3110_hw_tx(spi, frame);
priv->tx_len = 1 + frame->can_dlc;
can_put_echo_skb(priv->tx_skb, net, 0);
priv->tx_skb = NULL;
}
}
mutex_unlock(&priv->hi3110_lock);
}
static void hi3110_restart_work_handler(struct work_struct *ws)
{
struct hi3110_priv *priv = container_of(ws, struct hi3110_priv,
restart_work);
struct spi_device *spi = priv->spi;
struct net_device *net = priv->net;
mutex_lock(&priv->hi3110_lock);
if (priv->after_suspend) {
hi3110_hw_reset(spi);
hi3110_setup(net);
if (priv->after_suspend & HI3110_AFTER_SUSPEND_RESTART) {
hi3110_set_normal_mode(spi);
} else if (priv->after_suspend & HI3110_AFTER_SUSPEND_UP) {
netif_device_attach(net);
hi3110_clean(net);
hi3110_set_normal_mode(spi);
netif_wake_queue(net);
} else {
hi3110_hw_sleep(spi);
}
priv->after_suspend = 0;
priv->force_quit = 0;
}
if (priv->restart_tx) {
priv->restart_tx = 0;
hi3110_hw_reset(spi);
hi3110_setup(net);
hi3110_clean(net);
hi3110_set_normal_mode(spi);
netif_wake_queue(net);
}
mutex_unlock(&priv->hi3110_lock);
}
static irqreturn_t hi3110_can_ist(int irq, void *dev_id)
{
struct hi3110_priv *priv = dev_id;
struct spi_device *spi = priv->spi;
struct net_device *net = priv->net;
mutex_lock(&priv->hi3110_lock);
while (!priv->force_quit) {
enum can_state new_state;
u8 intf, eflag, statf;
while (!(HI3110_STAT_RXFMTY &
(statf = hi3110_read(spi, HI3110_READ_STATF)))) {
hi3110_hw_rx(spi);
}
intf = hi3110_read(spi, HI3110_READ_INTF);
eflag = hi3110_read(spi, HI3110_READ_ERR);
/* Update can state */
if (eflag & HI3110_ERR_BUSOFF)
new_state = CAN_STATE_BUS_OFF;
else if (eflag & HI3110_ERR_PASSIVE_MASK)
new_state = CAN_STATE_ERROR_PASSIVE;
else if (statf & HI3110_STAT_ERRW)
new_state = CAN_STATE_ERROR_WARNING;
else
new_state = CAN_STATE_ERROR_ACTIVE;
if (new_state != priv->can.state) {
struct can_frame *cf;
struct sk_buff *skb;
enum can_state rx_state, tx_state;
u8 rxerr, txerr;
skb = alloc_can_err_skb(net, &cf);
if (!skb)
break;
txerr = hi3110_read(spi, HI3110_READ_TEC);
rxerr = hi3110_read(spi, HI3110_READ_REC);
cf->data[6] = txerr;
cf->data[7] = rxerr;
tx_state = txerr >= rxerr ? new_state : 0;
rx_state = txerr <= rxerr ? new_state : 0;
can_change_state(net, cf, tx_state, rx_state);
netif_rx_ni(skb);
if (new_state == CAN_STATE_BUS_OFF) {
can_bus_off(net);
if (priv->can.restart_ms == 0) {
priv->force_quit = 1;
hi3110_hw_sleep(spi);
break;
}
}
}
/* Update bus errors */
if ((intf & HI3110_INT_BUSERR) &&
(priv->can.ctrlmode & CAN_CTRLMODE_BERR_REPORTING)) {
struct can_frame *cf;
struct sk_buff *skb;
/* Check for protocol errors */
if (eflag & HI3110_ERR_PROTOCOL_MASK) {
skb = alloc_can_err_skb(net, &cf);
if (!skb)
break;
cf->can_id |= CAN_ERR_PROT | CAN_ERR_BUSERROR;
priv->can.can_stats.bus_error++;
priv->net->stats.rx_errors++;
if (eflag & HI3110_ERR_BITERR)
cf->data[2] |= CAN_ERR_PROT_BIT;
else if (eflag & HI3110_ERR_FRMERR)
cf->data[2] |= CAN_ERR_PROT_FORM;
else if (eflag & HI3110_ERR_STUFERR)
cf->data[2] |= CAN_ERR_PROT_STUFF;
else if (eflag & HI3110_ERR_CRCERR)
cf->data[3] |= CAN_ERR_PROT_LOC_CRC_SEQ;
else if (eflag & HI3110_ERR_ACKERR)
cf->data[3] |= CAN_ERR_PROT_LOC_ACK;
cf->data[6] = hi3110_read(spi, HI3110_READ_TEC);
cf->data[7] = hi3110_read(spi, HI3110_READ_REC);
netdev_dbg(priv->net, "Bus Error\n");
netif_rx_ni(skb);
}
}
if (priv->tx_len && statf & HI3110_STAT_TXMTY) {
net->stats.tx_packets++;
net->stats.tx_bytes += priv->tx_len - 1;
can_led_event(net, CAN_LED_EVENT_TX);
if (priv->tx_len) {
can_get_echo_skb(net, 0);
priv->tx_len = 0;
}
netif_wake_queue(net);
}
if (intf == 0)
break;
}
mutex_unlock(&priv->hi3110_lock);
return IRQ_HANDLED;
}
static int hi3110_open(struct net_device *net)
{
struct hi3110_priv *priv = netdev_priv(net);
struct spi_device *spi = priv->spi;
unsigned long flags = IRQF_ONESHOT | IRQF_TRIGGER_HIGH;
int ret;
ret = open_candev(net);
if (ret)
return ret;
mutex_lock(&priv->hi3110_lock);
hi3110_power_enable(priv->transceiver, 1);
priv->force_quit = 0;
priv->tx_skb = NULL;
priv->tx_len = 0;
ret = request_threaded_irq(spi->irq, NULL, hi3110_can_ist,
flags, DEVICE_NAME, priv);
if (ret) {
dev_err(&spi->dev, "failed to acquire irq %d\n", spi->irq);
goto out_close;
}
priv->wq = alloc_workqueue("hi3110_wq", WQ_FREEZABLE | WQ_MEM_RECLAIM,
0);
if (!priv->wq) {
ret = -ENOMEM;
goto out_free_irq;
}
INIT_WORK(&priv->tx_work, hi3110_tx_work_handler);
INIT_WORK(&priv->restart_work, hi3110_restart_work_handler);
ret = hi3110_hw_reset(spi);
if (ret)
goto out_free_wq;
ret = hi3110_setup(net);
if (ret)
goto out_free_wq;
ret = hi3110_set_normal_mode(spi);
if (ret)
goto out_free_wq;
can_led_event(net, CAN_LED_EVENT_OPEN);
netif_wake_queue(net);
mutex_unlock(&priv->hi3110_lock);
return 0;
out_free_wq:
destroy_workqueue(priv->wq);
out_free_irq:
free_irq(spi->irq, priv);
hi3110_hw_sleep(spi);
out_close:
hi3110_power_enable(priv->transceiver, 0);
close_candev(net);
mutex_unlock(&priv->hi3110_lock);
return ret;
}
static const struct net_device_ops hi3110_netdev_ops = {
.ndo_open = hi3110_open,
.ndo_stop = hi3110_stop,
.ndo_start_xmit = hi3110_hard_start_xmit,
};
static const struct of_device_id hi3110_of_match[] = {
{
.compatible = "holt,hi3110",
.data = (void *)CAN_HI3110_HI3110,
},
{ }
};
MODULE_DEVICE_TABLE(of, hi3110_of_match);
static const struct spi_device_id hi3110_id_table[] = {
{
.name = "hi3110",
.driver_data = (kernel_ulong_t)CAN_HI3110_HI3110,
},
{ }
};
MODULE_DEVICE_TABLE(spi, hi3110_id_table);
static int hi3110_can_probe(struct spi_device *spi)
{
const struct of_device_id *of_id = of_match_device(hi3110_of_match,
&spi->dev);
struct net_device *net;
struct hi3110_priv *priv;
struct clk *clk;
int freq, ret;
clk = devm_clk_get(&spi->dev, NULL);
if (IS_ERR(clk)) {
dev_err(&spi->dev, "no CAN clock source defined\n");
return PTR_ERR(clk);
}
freq = clk_get_rate(clk);
/* Sanity check */
if (freq > 40000000)
return -ERANGE;
/* Allocate can/net device */
net = alloc_candev(sizeof(struct hi3110_priv), HI3110_TX_ECHO_SKB_MAX);
if (!net)
return -ENOMEM;
if (!IS_ERR(clk)) {
ret = clk_prepare_enable(clk);
if (ret)
goto out_free;
}
net->netdev_ops = &hi3110_netdev_ops;
net->flags |= IFF_ECHO;
priv = netdev_priv(net);
priv->can.bittiming_const = &hi3110_bittiming_const;
priv->can.do_set_mode = hi3110_do_set_mode;
priv->can.do_get_berr_counter = hi3110_get_berr_counter;
priv->can.clock.freq = freq / 2;
priv->can.ctrlmode_supported = CAN_CTRLMODE_3_SAMPLES |
CAN_CTRLMODE_LOOPBACK |
CAN_CTRLMODE_LISTENONLY |
CAN_CTRLMODE_BERR_REPORTING;
if (of_id)
priv->model = (enum hi3110_model)of_id->data;
else
priv->model = spi_get_device_id(spi)->driver_data;
priv->net = net;
priv->clk = clk;
spi_set_drvdata(spi, priv);
/* Configure the SPI bus */
spi->bits_per_word = 8;
ret = spi_setup(spi);
if (ret)
goto out_clk;
priv->power = devm_regulator_get_optional(&spi->dev, "vdd");
priv->transceiver = devm_regulator_get_optional(&spi->dev, "xceiver");
if ((PTR_ERR(priv->power) == -EPROBE_DEFER) ||
(PTR_ERR(priv->transceiver) == -EPROBE_DEFER)) {
ret = -EPROBE_DEFER;
goto out_clk;
}
ret = hi3110_power_enable(priv->power, 1);
if (ret)
goto out_clk;
priv->spi = spi;
mutex_init(&priv->hi3110_lock);
/* If requested, allocate DMA buffers */
if (hi3110_enable_dma) {
spi->dev.coherent_dma_mask = ~0;
/* Minimum coherent DMA allocation is PAGE_SIZE, so allocate
* that much and share it between Tx and Rx DMA buffers.
*/
priv->spi_tx_buf = dmam_alloc_coherent(&spi->dev,
PAGE_SIZE,
&priv->spi_tx_dma,
GFP_DMA);
if (priv->spi_tx_buf) {
priv->spi_rx_buf = (priv->spi_tx_buf + (PAGE_SIZE / 2));
priv->spi_rx_dma = (dma_addr_t)(priv->spi_tx_dma +
(PAGE_SIZE / 2));
} else {
/* Fall back to non-DMA */
hi3110_enable_dma = 0;
}
}
/* Allocate non-DMA buffers */
if (!hi3110_enable_dma) {
priv->spi_tx_buf = devm_kzalloc(&spi->dev, HI3110_RX_BUF_LEN,
GFP_KERNEL);
if (!priv->spi_tx_buf) {
ret = -ENOMEM;
goto error_probe;
}
priv->spi_rx_buf = devm_kzalloc(&spi->dev, HI3110_RX_BUF_LEN,
GFP_KERNEL);
if (!priv->spi_rx_buf) {
ret = -ENOMEM;
goto error_probe;
}
}
SET_NETDEV_DEV(net, &spi->dev);
ret = hi3110_hw_probe(spi);
if (ret) {
if (ret == -ENODEV)
dev_err(&spi->dev, "Cannot initialize %x. Wrong wiring?\n",
priv->model);
goto error_probe;
}
hi3110_hw_sleep(spi);
ret = register_candev(net);
if (ret)
goto error_probe;
devm_can_led_init(net);
netdev_info(net, "%x successfully initialized.\n", priv->model);
return 0;
error_probe:
hi3110_power_enable(priv->power, 0);
out_clk:
if (!IS_ERR(clk))
clk_disable_unprepare(clk);
out_free:
free_candev(net);
dev_err(&spi->dev, "Probe failed, err=%d\n", -ret);
return ret;
}
static int hi3110_can_remove(struct spi_device *spi)
{
struct hi3110_priv *priv = spi_get_drvdata(spi);
struct net_device *net = priv->net;
unregister_candev(net);
hi3110_power_enable(priv->power, 0);
if (!IS_ERR(priv->clk))
clk_disable_unprepare(priv->clk);
free_candev(net);
return 0;
}
static int __maybe_unused hi3110_can_suspend(struct device *dev)
{
struct spi_device *spi = to_spi_device(dev);
struct hi3110_priv *priv = spi_get_drvdata(spi);
struct net_device *net = priv->net;
priv->force_quit = 1;
disable_irq(spi->irq);
/* Note: at this point neither IST nor workqueues are running.
* open/stop cannot be called anyway so locking is not needed
*/
if (netif_running(net)) {
netif_device_detach(net);
hi3110_hw_sleep(spi);
hi3110_power_enable(priv->transceiver, 0);
priv->after_suspend = HI3110_AFTER_SUSPEND_UP;
} else {
priv->after_suspend = HI3110_AFTER_SUSPEND_DOWN;
}
if (!IS_ERR_OR_NULL(priv->power)) {
regulator_disable(priv->power);
priv->after_suspend |= HI3110_AFTER_SUSPEND_POWER;
}
return 0;
}
static int __maybe_unused hi3110_can_resume(struct device *dev)
{
struct spi_device *spi = to_spi_device(dev);
struct hi3110_priv *priv = spi_get_drvdata(spi);
if (priv->after_suspend & HI3110_AFTER_SUSPEND_POWER)
hi3110_power_enable(priv->power, 1);
if (priv->after_suspend & HI3110_AFTER_SUSPEND_UP) {
hi3110_power_enable(priv->transceiver, 1);
queue_work(priv->wq, &priv->restart_work);
} else {
priv->after_suspend = 0;
}
priv->force_quit = 0;
enable_irq(spi->irq);
return 0;
}
static SIMPLE_DEV_PM_OPS(hi3110_can_pm_ops, hi3110_can_suspend, hi3110_can_resume);
static struct spi_driver hi3110_can_driver = {
.driver = {
.name = DEVICE_NAME,
.of_match_table = hi3110_of_match,
.pm = &hi3110_can_pm_ops,
},
.id_table = hi3110_id_table,
.probe = hi3110_can_probe,
.remove = hi3110_can_remove,
};
module_spi_driver(hi3110_can_driver);
MODULE_AUTHOR("Akshay Bhat <akshay.bhat@timesys.com>");
MODULE_AUTHOR("Casey Fitzpatrick <casey.fitzpatrick@timesys.com>");
MODULE_DESCRIPTION("Holt HI-3110 CAN driver");
MODULE_LICENSE("GPL v2");
/*
* CAN bus driver for Microchip 251x/25625 CAN Controller with SPI Interface
*
* MCP2510 support and bug fixes by Christian Pellegrin
* <chripell@evolware.org>
*
* Copyright 2009 Christian Pellegrin EVOL S.r.l.
*
* Copyright 2007 Raymarine UK, Ltd. All Rights Reserved.
* Written under contract by:
* Chris Elston, Katalix Systems, Ltd.
*
* Based on Microchip MCP251x CAN controller driver written by
* David Vrabel, Copyright 2006 Arcom Control Systems Ltd.
*
* Based on CAN bus driver for the CCAN controller written by
* - Sascha Hauer, Marc Kleine-Budde, Pengutronix
* - Simon Kallweit, intefo AG
* Copyright 2007
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the version 2 of the GNU General Public License
* as published by the Free Software Foundation
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*
* You should have received a copy of the GNU General Public License
* along with this program; if not, see <http://www.gnu.org/licenses/>.
*
*
*
* Your platform definition file should specify something like:
*
* static struct mcp251x_platform_data mcp251x_info = {
* .oscillator_frequency = 8000000,
* };
*
* static struct spi_board_info spi_board_info[] = {
* {
* .modalias = "mcp2510",
* // "mcp2515" or "mcp25625" depending on your controller
* .platform_data = &mcp251x_info,
* .irq = IRQ_EINT13,
* .max_speed_hz = 2*1000*1000,
* .chip_select = 2,
* },
* };
*
* Please see mcp251x.h for a description of the fields in
* struct mcp251x_platform_data.
*
*/
#include <linux/can/core.h>
#include <linux/can/dev.h>
#include <linux/can/led.h>
#include <linux/can/platform/mcp251x.h>
#include <linux/clk.h>
#include <linux/completion.h>
#include <linux/delay.h>
#include <linux/device.h>
#include <linux/dma-mapping.h>
#include <linux/freezer.h>
#include <linux/interrupt.h>
#include <linux/io.h>
#include <linux/kernel.h>
#include <linux/module.h>
#include <linux/netdevice.h>
#include <linux/of.h>
#include <linux/of_device.h>
#include <linux/platform_device.h>
#include <linux/slab.h>
#include <linux/spi/spi.h>
#include <linux/uaccess.h>
#include <linux/regulator/consumer.h>
/* SPI interface instruction set */
#define INSTRUCTION_WRITE 0x02
#define INSTRUCTION_READ 0x03
#define INSTRUCTION_BIT_MODIFY 0x05
#define INSTRUCTION_LOAD_TXB(n) (0x40 + 2 * (n))
#define INSTRUCTION_READ_RXB(n) (((n) == 0) ? 0x90 : 0x94)
#define INSTRUCTION_RESET 0xC0
#define RTS_TXB0 0x01
#define RTS_TXB1 0x02
#define RTS_TXB2 0x04
#define INSTRUCTION_RTS(n) (0x80 | ((n) & 0x07))
/* MPC251x registers */
#define CANSTAT 0x0e
#define CANCTRL 0x0f
# define CANCTRL_REQOP_MASK 0xe0
# define CANCTRL_REQOP_CONF 0x80
# define CANCTRL_REQOP_LISTEN_ONLY 0x60
# define CANCTRL_REQOP_LOOPBACK 0x40
# define CANCTRL_REQOP_SLEEP 0x20
# define CANCTRL_REQOP_NORMAL 0x00
# define CANCTRL_OSM 0x08
# define CANCTRL_ABAT 0x10
#define TEC 0x1c
#define REC 0x1d
#define CNF1 0x2a
# define CNF1_SJW_SHIFT 6
#define CNF2 0x29
# define CNF2_BTLMODE 0x80
# define CNF2_SAM 0x40
# define CNF2_PS1_SHIFT 3
#define CNF3 0x28
# define CNF3_SOF 0x08
# define CNF3_WAKFIL 0x04
# define CNF3_PHSEG2_MASK 0x07
#define CANINTE 0x2b
# define CANINTE_MERRE 0x80
# define CANINTE_WAKIE 0x40
# define CANINTE_ERRIE 0x20
# define CANINTE_TX2IE 0x10
# define CANINTE_TX1IE 0x08
# define CANINTE_TX0IE 0x04
# define CANINTE_RX1IE 0x02
# define CANINTE_RX0IE 0x01
#define CANINTF 0x2c
# define CANINTF_MERRF 0x80
# define CANINTF_WAKIF 0x40
# define CANINTF_ERRIF 0x20
# define CANINTF_TX2IF 0x10
# define CANINTF_TX1IF 0x08
# define CANINTF_TX0IF 0x04
# define CANINTF_RX1IF 0x02
# define CANINTF_RX0IF 0x01
# define CANINTF_RX (CANINTF_RX0IF | CANINTF_RX1IF)
# define CANINTF_TX (CANINTF_TX2IF | CANINTF_TX1IF | CANINTF_TX0IF)
# define CANINTF_ERR (CANINTF_ERRIF)
#define EFLG 0x2d
# define EFLG_EWARN 0x01
# define EFLG_RXWAR 0x02
# define EFLG_TXWAR 0x04
# define EFLG_RXEP 0x08
# define EFLG_TXEP 0x10
# define EFLG_TXBO 0x20
# define EFLG_RX0OVR 0x40
# define EFLG_RX1OVR 0x80
#define TXBCTRL(n) (((n) * 0x10) + 0x30 + TXBCTRL_OFF)
# define TXBCTRL_ABTF 0x40
# define TXBCTRL_MLOA 0x20
# define TXBCTRL_TXERR 0x10
# define TXBCTRL_TXREQ 0x08
#define TXBSIDH(n) (((n) * 0x10) + 0x30 + TXBSIDH_OFF)
# define SIDH_SHIFT 3
#define TXBSIDL(n) (((n) * 0x10) + 0x30 + TXBSIDL_OFF)
# define SIDL_SID_MASK 7
# define SIDL_SID_SHIFT 5
# define SIDL_EXIDE_SHIFT 3
# define SIDL_EID_SHIFT 16
# define SIDL_EID_MASK 3
#define TXBEID8(n) (((n) * 0x10) + 0x30 + TXBEID8_OFF)
#define TXBEID0(n) (((n) * 0x10) + 0x30 + TXBEID0_OFF)
#define TXBDLC(n) (((n) * 0x10) + 0x30 + TXBDLC_OFF)
# define DLC_RTR_SHIFT 6
#define TXBCTRL_OFF 0
#define TXBSIDH_OFF 1
#define TXBSIDL_OFF 2
#define TXBEID8_OFF 3
#define TXBEID0_OFF 4
#define TXBDLC_OFF 5
#define TXBDAT_OFF 6
#define RXBCTRL(n) (((n) * 0x10) + 0x60 + RXBCTRL_OFF)
# define RXBCTRL_BUKT 0x04
# define RXBCTRL_RXM0 0x20
# define RXBCTRL_RXM1 0x40
#define RXBSIDH(n) (((n) * 0x10) + 0x60 + RXBSIDH_OFF)
# define RXBSIDH_SHIFT 3
#define RXBSIDL(n) (((n) * 0x10) + 0x60 + RXBSIDL_OFF)
# define RXBSIDL_IDE 0x08
# define RXBSIDL_SRR 0x10
# define RXBSIDL_EID 3
# define RXBSIDL_SHIFT 5
#define RXBEID8(n) (((n) * 0x10) + 0x60 + RXBEID8_OFF)
#define RXBEID0(n) (((n) * 0x10) + 0x60 + RXBEID0_OFF)
#define RXBDLC(n) (((n) * 0x10) + 0x60 + RXBDLC_OFF)
# define RXBDLC_LEN_MASK 0x0f
# define RXBDLC_RTR 0x40
#define RXBCTRL_OFF 0
#define RXBSIDH_OFF 1
#define RXBSIDL_OFF 2
#define RXBEID8_OFF 3
#define RXBEID0_OFF 4
#define RXBDLC_OFF 5
#define RXBDAT_OFF 6
#define RXFSID(n) ((n < 3) ? 0 : 4)
#define RXFSIDH(n) ((n) * 4 + RXFSID(n))
#define RXFSIDL(n) ((n) * 4 + 1 + RXFSID(n))
#define RXFEID8(n) ((n) * 4 + 2 + RXFSID(n))
#define RXFEID0(n) ((n) * 4 + 3 + RXFSID(n))
#define RXMSIDH(n) ((n) * 4 + 0x20)
#define RXMSIDL(n) ((n) * 4 + 0x21)
#define RXMEID8(n) ((n) * 4 + 0x22)
#define RXMEID0(n) ((n) * 4 + 0x23)
#define GET_BYTE(val, byte) \
(((val) >> ((byte) * 8)) & 0xff)
#define SET_BYTE(val, byte) \
(((val) & 0xff) << ((byte) * 8))
/*
* Buffer size required for the largest SPI transfer (i.e., reading a
* frame)
*/
#define CAN_FRAME_MAX_DATA_LEN 8
#define SPI_TRANSFER_BUF_LEN (6 + CAN_FRAME_MAX_DATA_LEN)
#define CAN_FRAME_MAX_BITS 128
#define TX_ECHO_SKB_MAX 1
#define MCP251X_OST_DELAY_MS (5)
#define DEVICE_NAME "mcp251x"
static int mcp251x_enable_dma; /* Enable SPI DMA. Default: 0 (Off) */
module_param(mcp251x_enable_dma, int, 0444);
MODULE_PARM_DESC(mcp251x_enable_dma, "Enable SPI DMA. Default: 0 (Off)");
static const struct can_bittiming_const mcp251x_bittiming_const = {
.name = DEVICE_NAME,
.tseg1_min = 3,
.tseg1_max = 16,
.tseg2_min = 2,
.tseg2_max = 8,
.sjw_max = 4,
.brp_min = 1,
.brp_max = 64,
.brp_inc = 1,
};
enum mcp251x_model {
CAN_MCP251X_MCP2510 = 0x2510,
CAN_MCP251X_MCP2515 = 0x2515,
CAN_MCP251X_MCP25625 = 0x25625,
};
struct mcp251x_priv {
struct can_priv can;
struct net_device *net;
struct spi_device *spi;
enum mcp251x_model model;
struct mutex mcp_lock; /* SPI device lock */
u8 *spi_tx_buf;
u8 *spi_rx_buf;
dma_addr_t spi_tx_dma;
dma_addr_t spi_rx_dma;
struct sk_buff *tx_skb;
int tx_len;
struct workqueue_struct *wq;
struct work_struct tx_work;
struct work_struct restart_work;
int force_quit;
int after_suspend;
#define AFTER_SUSPEND_UP 1
#define AFTER_SUSPEND_DOWN 2
#define AFTER_SUSPEND_POWER 4
#define AFTER_SUSPEND_RESTART 8
int restart_tx;
struct regulator *power;
struct regulator *transceiver;
struct clk *clk;
};
#define MCP251X_IS(_model) \
static inline int mcp251x_is_##_model(struct spi_device *spi) \
{ \
struct mcp251x_priv *priv = spi_get_drvdata(spi); \
return priv->model == CAN_MCP251X_MCP##_model; \
}
MCP251X_IS(2510);
static void mcp251x_clean(struct net_device *net)
{
struct mcp251x_priv *priv = netdev_priv(net);
if (priv->tx_skb || priv->tx_len)
net->stats.tx_errors++;
if (priv->tx_skb)
dev_kfree_skb(priv->tx_skb);
if (priv->tx_len)
can_free_echo_skb(priv->net, 0);
priv->tx_skb = NULL;
priv->tx_len = 0;
}
/*
* Note about handling of error return of mcp251x_spi_trans: accessing
* registers via SPI is not really different conceptually than using
* normal I/O assembler instructions, although it's much more
* complicated from a practical POV. So it's not advisable to always
* check the return value of this function. Imagine that every
* read{b,l}, write{b,l} and friends would be bracketed in "if ( < 0)
* error();", it would be a great mess (well there are some situation
* when exception handling C++ like could be useful after all). So we
* just check that transfers are OK at the beginning of our
* conversation with the chip and to avoid doing really nasty things
* (like injecting bogus packets in the network stack).
*/
static int mcp251x_spi_trans(struct spi_device *spi, int len)
{
struct mcp251x_priv *priv = spi_get_drvdata(spi);
struct spi_transfer t = {
.tx_buf = priv->spi_tx_buf,
.rx_buf = priv->spi_rx_buf,
.len = len,
.cs_change = 0,
};
struct spi_message m;
int ret;
spi_message_init(&m);
if (mcp251x_enable_dma) {
t.tx_dma = priv->spi_tx_dma;
t.rx_dma = priv->spi_rx_dma;
m.is_dma_mapped = 1;
}
spi_message_add_tail(&t, &m);
ret = spi_sync(spi, &m);
if (ret)
dev_err(&spi->dev, "spi transfer failed: ret = %d\n", ret);
return ret;
}
static u8 mcp251x_read_reg(struct spi_device *spi, uint8_t reg)
{
struct mcp251x_priv *priv = spi_get_drvdata(spi);
u8 val = 0;
priv->spi_tx_buf[0] = INSTRUCTION_READ;
priv->spi_tx_buf[1] = reg;
mcp251x_spi_trans(spi, 3);
val = priv->spi_rx_buf[2];
return val;
}
static void mcp251x_read_2regs(struct spi_device *spi, uint8_t reg,
uint8_t *v1, uint8_t *v2)
{
struct mcp251x_priv *priv = spi_get_drvdata(spi);
priv->spi_tx_buf[0] = INSTRUCTION_READ;
priv->spi_tx_buf[1] = reg;
mcp251x_spi_trans(spi, 4);
*v1 = priv->spi_rx_buf[2];
*v2 = priv->spi_rx_buf[3];
}
static void mcp251x_write_reg(struct spi_device *spi, u8 reg, uint8_t val)
{
struct mcp251x_priv *priv = spi_get_drvdata(spi);
priv->spi_tx_buf[0] = INSTRUCTION_WRITE;
priv->spi_tx_buf[1] = reg;
priv->spi_tx_buf[2] = val;
mcp251x_spi_trans(spi, 3);
}
static void mcp251x_write_bits(struct spi_device *spi, u8 reg,
u8 mask, uint8_t val)
{
struct mcp251x_priv *priv = spi_get_drvdata(spi);
priv->spi_tx_buf[0] = INSTRUCTION_BIT_MODIFY;
priv->spi_tx_buf[1] = reg;
priv->spi_tx_buf[2] = mask;
priv->spi_tx_buf[3] = val;
mcp251x_spi_trans(spi, 4);
}
static void mcp251x_hw_tx_frame(struct spi_device *spi, u8 *buf,
int len, int tx_buf_idx)
{
struct mcp251x_priv *priv = spi_get_drvdata(spi);
if (mcp251x_is_2510(spi)) {
int i;
for (i = 1; i < TXBDAT_OFF + len; i++)
mcp251x_write_reg(spi, TXBCTRL(tx_buf_idx) + i,
buf[i]);
} else {
memcpy(priv->spi_tx_buf, buf, TXBDAT_OFF + len);
mcp251x_spi_trans(spi, TXBDAT_OFF + len);
}
}
static void mcp251x_hw_tx(struct spi_device *spi, struct can_frame *frame,
int tx_buf_idx)
{
struct mcp251x_priv *priv = spi_get_drvdata(spi);
u32 sid, eid, exide, rtr;
u8 buf[SPI_TRANSFER_BUF_LEN];
exide = (frame->can_id & CAN_EFF_FLAG) ? 1 : 0; /* Extended ID Enable */
if (exide)
sid = (frame->can_id & CAN_EFF_MASK) >> 18;
else
sid = frame->can_id & CAN_SFF_MASK; /* Standard ID */
eid = frame->can_id & CAN_EFF_MASK; /* Extended ID */
rtr = (frame->can_id & CAN_RTR_FLAG) ? 1 : 0; /* Remote transmission */
buf[TXBCTRL_OFF] = INSTRUCTION_LOAD_TXB(tx_buf_idx);
buf[TXBSIDH_OFF] = sid >> SIDH_SHIFT;
buf[TXBSIDL_OFF] = ((sid & SIDL_SID_MASK) << SIDL_SID_SHIFT) |
(exide << SIDL_EXIDE_SHIFT) |
((eid >> SIDL_EID_SHIFT) & SIDL_EID_MASK);
buf[TXBEID8_OFF] = GET_BYTE(eid, 1);
buf[TXBEID0_OFF] = GET_BYTE(eid, 0);
buf[TXBDLC_OFF] = (rtr << DLC_RTR_SHIFT) | frame->can_dlc;
memcpy(buf + TXBDAT_OFF, frame->data, frame->can_dlc);
mcp251x_hw_tx_frame(spi, buf, frame->can_dlc, tx_buf_idx);
/* use INSTRUCTION_RTS, to avoid "repeated frame problem" */
priv->spi_tx_buf[0] = INSTRUCTION_RTS(1 << tx_buf_idx);
mcp251x_spi_trans(priv->spi, 1);
}
static void mcp251x_hw_rx_frame(struct spi_device *spi, u8 *buf,
int buf_idx)
{
struct mcp251x_priv *priv = spi_get_drvdata(spi);
if (mcp251x_is_2510(spi)) {
int i, len;
for (i = 1; i < RXBDAT_OFF; i++)
buf[i] = mcp251x_read_reg(spi, RXBCTRL(buf_idx) + i);
len = get_can_dlc(buf[RXBDLC_OFF] & RXBDLC_LEN_MASK);
for (; i < (RXBDAT_OFF + len); i++)
buf[i] = mcp251x_read_reg(spi, RXBCTRL(buf_idx) + i);
} else {
priv->spi_tx_buf[RXBCTRL_OFF] = INSTRUCTION_READ_RXB(buf_idx);
mcp251x_spi_trans(spi, SPI_TRANSFER_BUF_LEN);
memcpy(buf, priv->spi_rx_buf, SPI_TRANSFER_BUF_LEN);
}
}
static void mcp251x_hw_rx(struct spi_device *spi, int buf_idx)
{
struct mcp251x_priv *priv = spi_get_drvdata(spi);
struct sk_buff *skb;
struct can_frame *frame;
u8 buf[SPI_TRANSFER_BUF_LEN];
skb = alloc_can_skb(priv->net, &frame);
if (!skb) {
dev_err(&spi->dev, "cannot allocate RX skb\n");
priv->net->stats.rx_dropped++;
return;
}
mcp251x_hw_rx_frame(spi, buf, buf_idx);
if (buf[RXBSIDL_OFF] & RXBSIDL_IDE) {
/* Extended ID format */
frame->can_id = CAN_EFF_FLAG;
frame->can_id |=
/* Extended ID part */
SET_BYTE(buf[RXBSIDL_OFF] & RXBSIDL_EID, 2) |
SET_BYTE(buf[RXBEID8_OFF], 1) |
SET_BYTE(buf[RXBEID0_OFF], 0) |
/* Standard ID part */
(((buf[RXBSIDH_OFF] << RXBSIDH_SHIFT) |
(buf[RXBSIDL_OFF] >> RXBSIDL_SHIFT)) << 18);
/* Remote transmission request */
if (buf[RXBDLC_OFF] & RXBDLC_RTR)
frame->can_id |= CAN_RTR_FLAG;
} else {
/* Standard ID format */
frame->can_id =
(buf[RXBSIDH_OFF] << RXBSIDH_SHIFT) |
(buf[RXBSIDL_OFF] >> RXBSIDL_SHIFT);
if (buf[RXBSIDL_OFF] & RXBSIDL_SRR)
frame->can_id |= CAN_RTR_FLAG;
}
/* Data length */
frame->can_dlc = get_can_dlc(buf[RXBDLC_OFF] & RXBDLC_LEN_MASK);
memcpy(frame->data, buf + RXBDAT_OFF, frame->can_dlc);
priv->net->stats.rx_packets++;
priv->net->stats.rx_bytes += frame->can_dlc;
can_led_event(priv->net, CAN_LED_EVENT_RX);
netif_rx_ni(skb);
}
static void mcp251x_hw_sleep(struct spi_device *spi)
{
mcp251x_write_reg(spi, CANCTRL, CANCTRL_REQOP_SLEEP);
}
static netdev_tx_t mcp251x_hard_start_xmit(struct sk_buff *skb,
struct net_device *net)
{
struct mcp251x_priv *priv = netdev_priv(net);
struct spi_device *spi = priv->spi;
if (priv->tx_skb || priv->tx_len) {
dev_warn(&spi->dev, "hard_xmit called while tx busy\n");
return NETDEV_TX_BUSY;
}
if (can_dropped_invalid_skb(net, skb))
return NETDEV_TX_OK;
netif_stop_queue(net);
priv->tx_skb = skb;
queue_work(priv->wq, &priv->tx_work);
return NETDEV_TX_OK;
}
static int mcp251x_do_set_mode(struct net_device *net, enum can_mode mode)
{
struct mcp251x_priv *priv = netdev_priv(net);
switch (mode) {
case CAN_MODE_START:
mcp251x_clean(net);
/* We have to delay work since SPI I/O may sleep */
priv->can.state = CAN_STATE_ERROR_ACTIVE;
priv->restart_tx = 1;
if (priv->can.restart_ms == 0)
priv->after_suspend = AFTER_SUSPEND_RESTART;
queue_work(priv->wq, &priv->restart_work);
break;
default:
return -EOPNOTSUPP;
}
return 0;
}
static int mcp251x_set_normal_mode(struct spi_device *spi)
{
struct mcp251x_priv *priv = spi_get_drvdata(spi);
unsigned long timeout;
/* Enable interrupts */
mcp251x_write_reg(spi, CANINTE,
CANINTE_ERRIE | CANINTE_TX2IE | CANINTE_TX1IE |
CANINTE_TX0IE | CANINTE_RX1IE | CANINTE_RX0IE);
if (priv->can.ctrlmode & CAN_CTRLMODE_LOOPBACK) {
/* Put device into loopback mode */
mcp251x_write_reg(spi, CANCTRL, CANCTRL_REQOP_LOOPBACK);
} else if (priv->can.ctrlmode & CAN_CTRLMODE_LISTENONLY) {
/* Put device into listen-only mode */
mcp251x_write_reg(spi, CANCTRL, CANCTRL_REQOP_LISTEN_ONLY);
} else {
/* Put device into normal mode */
mcp251x_write_reg(spi, CANCTRL, CANCTRL_REQOP_NORMAL);
/* Wait for the device to enter normal mode */
timeout = jiffies + HZ;
while (mcp251x_read_reg(spi, CANSTAT) & CANCTRL_REQOP_MASK) {
schedule();
if (time_after(jiffies, timeout)) {
dev_err(&spi->dev, "MCP251x didn't"
" enter in normal mode\n");
return -EBUSY;
}
}
}
priv->can.state = CAN_STATE_ERROR_ACTIVE;
return 0;
}
static int mcp251x_do_set_bittiming(struct net_device *net)
{
struct mcp251x_priv *priv = netdev_priv(net);
struct can_bittiming *bt = &priv->can.bittiming;
struct spi_device *spi = priv->spi;
mcp251x_write_reg(spi, CNF1, ((bt->sjw - 1) << CNF1_SJW_SHIFT) |
(bt->brp - 1));
mcp251x_write_reg(spi, CNF2, CNF2_BTLMODE |
(priv->can.ctrlmode & CAN_CTRLMODE_3_SAMPLES ?
CNF2_SAM : 0) |
((bt->phase_seg1 - 1) << CNF2_PS1_SHIFT) |
(bt->prop_seg - 1));
mcp251x_write_bits(spi, CNF3, CNF3_PHSEG2_MASK,
(bt->phase_seg2 - 1));
dev_dbg(&spi->dev, "CNF: 0x%02x 0x%02x 0x%02x\n",
mcp251x_read_reg(spi, CNF1),
mcp251x_read_reg(spi, CNF2),
mcp251x_read_reg(spi, CNF3));
return 0;
}
static int mcp251x_setup(struct net_device *net, struct spi_device *spi)
{
mcp251x_do_set_bittiming(net);
mcp251x_write_reg(spi, RXBCTRL(0),
RXBCTRL_BUKT | RXBCTRL_RXM0 | RXBCTRL_RXM1);
mcp251x_write_reg(spi, RXBCTRL(1),
RXBCTRL_RXM0 | RXBCTRL_RXM1);
return 0;
}
static int mcp251x_hw_reset(struct spi_device *spi)
{
struct mcp251x_priv *priv = spi_get_drvdata(spi);
unsigned long timeout;
int ret;
/* Wait for oscillator startup timer after power up */
mdelay(MCP251X_OST_DELAY_MS);
priv->spi_tx_buf[0] = INSTRUCTION_RESET;
ret = mcp251x_spi_trans(spi, 1);
if (ret)
return ret;
/* Wait for oscillator startup timer after reset */
mdelay(MCP251X_OST_DELAY_MS);
/* Wait for reset to finish */
timeout = jiffies + HZ;
while ((mcp251x_read_reg(spi, CANSTAT) & CANCTRL_REQOP_MASK) !=
CANCTRL_REQOP_CONF) {
usleep_range(MCP251X_OST_DELAY_MS * 1000,
MCP251X_OST_DELAY_MS * 1000 * 2);
if (time_after(jiffies, timeout)) {
dev_err(&spi->dev,
"MCP251x didn't enter in conf mode after reset\n");
return -EBUSY;
}
}
return 0;
}
static int mcp251x_hw_probe(struct spi_device *spi)
{
u8 ctrl;
int ret;
ret = mcp251x_hw_reset(spi);
if (ret)
return ret;
ctrl = mcp251x_read_reg(spi, CANCTRL);
dev_dbg(&spi->dev, "CANCTRL 0x%02x\n", ctrl);
/* Check for power up default value */
if ((ctrl & 0x17) != 0x07)
return -ENODEV;
return 0;
}
static int mcp251x_power_enable(struct regulator *reg, int enable)
{
if (IS_ERR_OR_NULL(reg))
return 0;
if (enable)
return regulator_enable(reg);
else
return regulator_disable(reg);
}
static int mcp251x_stop(struct net_device *net)
{
struct mcp251x_priv *priv = netdev_priv(net);
struct spi_device *spi = priv->spi;
close_candev(net);
priv->force_quit = 1;
free_irq(spi->irq, priv);
destroy_workqueue(priv->wq);
priv->wq = NULL;
mutex_lock(&priv->mcp_lock);
/* Disable and clear pending interrupts */
mcp251x_write_reg(spi, CANINTE, 0x00);
mcp251x_write_reg(spi, CANINTF, 0x00);
mcp251x_write_reg(spi, TXBCTRL(0), 0);
mcp251x_clean(net);
mcp251x_hw_sleep(spi);
mcp251x_power_enable(priv->transceiver, 0);
priv->can.state = CAN_STATE_STOPPED;
mutex_unlock(&priv->mcp_lock);
can_led_event(net, CAN_LED_EVENT_STOP);
return 0;
}
static void mcp251x_error_skb(struct net_device *net, int can_id, int data1)
{
struct sk_buff *skb;
struct can_frame *frame;
skb = alloc_can_err_skb(net, &frame);
if (skb) {
frame->can_id |= can_id;
frame->data[1] = data1;
netif_rx_ni(skb);
} else {
netdev_err(net, "cannot allocate error skb\n");
}
}
static void mcp251x_tx_work_handler(struct work_struct *ws)
{
struct mcp251x_priv *priv = container_of(ws, struct mcp251x_priv,
tx_work);
struct spi_device *spi = priv->spi;
struct net_device *net = priv->net;
struct can_frame *frame;
mutex_lock(&priv->mcp_lock);
if (priv->tx_skb) {
if (priv->can.state == CAN_STATE_BUS_OFF) {
mcp251x_clean(net);
} else {
frame = (struct can_frame *)priv->tx_skb->data;
if (frame->can_dlc > CAN_FRAME_MAX_DATA_LEN)
frame->can_dlc = CAN_FRAME_MAX_DATA_LEN;
mcp251x_hw_tx(spi, frame, 0);
priv->tx_len = 1 + frame->can_dlc;
can_put_echo_skb(priv->tx_skb, net, 0);
priv->tx_skb = NULL;
}
}
mutex_unlock(&priv->mcp_lock);
}
static void mcp251x_restart_work_handler(struct work_struct *ws)
{
struct mcp251x_priv *priv = container_of(ws, struct mcp251x_priv,
restart_work);
struct spi_device *spi = priv->spi;
struct net_device *net = priv->net;
mutex_lock(&priv->mcp_lock);
if (priv->after_suspend) {
mcp251x_hw_reset(spi);
mcp251x_setup(net, spi);
priv->force_quit = 0;
if (priv->after_suspend & AFTER_SUSPEND_RESTART) {
mcp251x_set_normal_mode(spi);
} else if (priv->after_suspend & AFTER_SUSPEND_UP) {
netif_device_attach(net);
mcp251x_clean(net);
mcp251x_set_normal_mode(spi);
netif_wake_queue(net);
} else {
mcp251x_hw_sleep(spi);
}
priv->after_suspend = 0;
}
if (priv->restart_tx) {
priv->restart_tx = 0;
mcp251x_write_reg(spi, TXBCTRL(0), 0);
mcp251x_clean(net);
netif_wake_queue(net);
mcp251x_error_skb(net, CAN_ERR_RESTARTED, 0);
}
mutex_unlock(&priv->mcp_lock);
}
static irqreturn_t mcp251x_can_ist(int irq, void *dev_id)
{
struct mcp251x_priv *priv = dev_id;
struct spi_device *spi = priv->spi;
struct net_device *net = priv->net;
mutex_lock(&priv->mcp_lock);
while (!priv->force_quit) {
enum can_state new_state;
u8 intf, eflag;
u8 clear_intf = 0;
int can_id = 0, data1 = 0;
mcp251x_read_2regs(spi, CANINTF, &intf, &eflag);
/* mask out flags we don't care about */
intf &= CANINTF_RX | CANINTF_TX | CANINTF_ERR;
/* receive buffer 0 */
if (intf & CANINTF_RX0IF) {
mcp251x_hw_rx(spi, 0);
/* Free one buffer ASAP
* (The MCP2515/25625 does this automatically.)
*/
if (mcp251x_is_2510(spi))
mcp251x_write_bits(spi, CANINTF, CANINTF_RX0IF, 0x00);
}
/* receive buffer 1 */
if (intf & CANINTF_RX1IF) {
mcp251x_hw_rx(spi, 1);
/* The MCP2515/25625 does this automatically. */
if (mcp251x_is_2510(spi))
clear_intf |= CANINTF_RX1IF;
}
/* any error or tx interrupt we need to clear? */
if (intf & (CANINTF_ERR | CANINTF_TX))
clear_intf |= intf & (CANINTF_ERR | CANINTF_TX);
if (clear_intf)
mcp251x_write_bits(spi, CANINTF, clear_intf, 0x00);
if (eflag & (EFLG_RX0OVR | EFLG_RX1OVR))
mcp251x_write_bits(spi, EFLG, eflag, 0x00);
/* Update can state */
if (eflag & EFLG_TXBO) {
new_state = CAN_STATE_BUS_OFF;
can_id |= CAN_ERR_BUSOFF;
} else if (eflag & EFLG_TXEP) {
new_state = CAN_STATE_ERROR_PASSIVE;
can_id |= CAN_ERR_CRTL;
data1 |= CAN_ERR_CRTL_TX_PASSIVE;
} else if (eflag & EFLG_RXEP) {
new_state = CAN_STATE_ERROR_PASSIVE;
can_id |= CAN_ERR_CRTL;
data1 |= CAN_ERR_CRTL_RX_PASSIVE;
} else if (eflag & EFLG_TXWAR) {
new_state = CAN_STATE_ERROR_WARNING;
can_id |= CAN_ERR_CRTL;
data1 |= CAN_ERR_CRTL_TX_WARNING;
} else if (eflag & EFLG_RXWAR) {
new_state = CAN_STATE_ERROR_WARNING;
can_id |= CAN_ERR_CRTL;
data1 |= CAN_ERR_CRTL_RX_WARNING;
} else {
new_state = CAN_STATE_ERROR_ACTIVE;
}
/* Update can state statistics */
switch (priv->can.state) {
case CAN_STATE_ERROR_ACTIVE:
if (new_state >= CAN_STATE_ERROR_WARNING &&
new_state <= CAN_STATE_BUS_OFF)
priv->can.can_stats.error_warning++;
case CAN_STATE_ERROR_WARNING: /* fallthrough */
if (new_state >= CAN_STATE_ERROR_PASSIVE &&
new_state <= CAN_STATE_BUS_OFF)
priv->can.can_stats.error_passive++;
break;
default:
break;
}
priv->can.state = new_state;
if (intf & CANINTF_ERRIF) {
/* Handle overflow counters */
if (eflag & (EFLG_RX0OVR | EFLG_RX1OVR)) {
if (eflag & EFLG_RX0OVR) {
net->stats.rx_over_errors++;
net->stats.rx_errors++;
}
if (eflag & EFLG_RX1OVR) {
net->stats.rx_over_errors++;
net->stats.rx_errors++;
}
can_id |= CAN_ERR_CRTL;
data1 |= CAN_ERR_CRTL_RX_OVERFLOW;
}
mcp251x_error_skb(net, can_id, data1);
}
if (priv->can.state == CAN_STATE_BUS_OFF) {
if (priv->can.restart_ms == 0) {
priv->force_quit = 1;
priv->can.can_stats.bus_off++;
can_bus_off(net);
mcp251x_hw_sleep(spi);
break;
}
}
if (intf == 0)
break;
if (intf & CANINTF_TX) {
net->stats.tx_packets++;
net->stats.tx_bytes += priv->tx_len - 1;
can_led_event(net, CAN_LED_EVENT_TX);
if (priv->tx_len) {
can_get_echo_skb(net, 0);
priv->tx_len = 0;
}
netif_wake_queue(net);
}
}
mutex_unlock(&priv->mcp_lock);
return IRQ_HANDLED;
}
static int mcp251x_open(struct net_device *net)
{
struct mcp251x_priv *priv = netdev_priv(net);
struct spi_device *spi = priv->spi;
unsigned long flags = IRQF_ONESHOT | IRQF_TRIGGER_FALLING;
int ret;
ret = open_candev(net);
if (ret) {
dev_err(&spi->dev, "unable to set initial baudrate!\n");
return ret;
}
mutex_lock(&priv->mcp_lock);
mcp251x_power_enable(priv->transceiver, 1);
priv->force_quit = 0;
priv->tx_skb = NULL;
priv->tx_len = 0;
ret = request_threaded_irq(spi->irq, NULL, mcp251x_can_ist,
flags | IRQF_ONESHOT, DEVICE_NAME, priv);
if (ret) {
dev_err(&spi->dev, "failed to acquire irq %d\n", spi->irq);
goto out_close;
}
priv->wq = alloc_workqueue("mcp251x_wq", WQ_FREEZABLE | WQ_MEM_RECLAIM,
0);
if (!priv->wq) {
ret = -ENOMEM;
goto out_clean;
}
INIT_WORK(&priv->tx_work, mcp251x_tx_work_handler);
INIT_WORK(&priv->restart_work, mcp251x_restart_work_handler);
ret = mcp251x_hw_reset(spi);
if (ret)
goto out_free_wq;
ret = mcp251x_setup(net, spi);
if (ret)
goto out_free_wq;
ret = mcp251x_set_normal_mode(spi);
if (ret)
goto out_free_wq;
can_led_event(net, CAN_LED_EVENT_OPEN);
netif_wake_queue(net);
mutex_unlock(&priv->mcp_lock);
return 0;
out_free_wq:
destroy_workqueue(priv->wq);
out_clean:
free_irq(spi->irq, priv);
mcp251x_hw_sleep(spi);
out_close:
mcp251x_power_enable(priv->transceiver, 0);
close_candev(net);
mutex_unlock(&priv->mcp_lock);
return ret;
}
static const struct net_device_ops mcp251x_netdev_ops = {
.ndo_open = mcp251x_open,
.ndo_stop = mcp251x_stop,
.ndo_start_xmit = mcp251x_hard_start_xmit,
.ndo_change_mtu = can_change_mtu,
};
static const struct of_device_id mcp251x_of_match[] = {
{
.compatible = "microchip,mcp2510",
.data = (void *)CAN_MCP251X_MCP2510,
},
{
.compatible = "microchip,mcp2515",
.data = (void *)CAN_MCP251X_MCP2515,
},
{
.compatible = "microchip,mcp25625",
.data = (void *)CAN_MCP251X_MCP25625,
},
{ }
};
MODULE_DEVICE_TABLE(of, mcp251x_of_match);
static const struct spi_device_id mcp251x_id_table[] = {
{
.name = "mcp2510",
.driver_data = (kernel_ulong_t)CAN_MCP251X_MCP2510,
},
{
.name = "mcp2515",
.driver_data = (kernel_ulong_t)CAN_MCP251X_MCP2515,
},
{
.name = "mcp25625",
.driver_data = (kernel_ulong_t)CAN_MCP251X_MCP25625,
},
{ }
};
MODULE_DEVICE_TABLE(spi, mcp251x_id_table);
static int mcp251x_can_probe(struct spi_device *spi)
{
const struct of_device_id *of_id = of_match_device(mcp251x_of_match,
&spi->dev);
struct mcp251x_platform_data *pdata = dev_get_platdata(&spi->dev);
struct net_device *net;
struct mcp251x_priv *priv;
struct clk *clk;
int freq, ret;
clk = devm_clk_get(&spi->dev, NULL);
if (IS_ERR(clk)) {
if (pdata)
freq = pdata->oscillator_frequency;
else
return PTR_ERR(clk);
} else {
freq = clk_get_rate(clk);
}
/* Sanity check */
if (freq < 1000000 || freq > 25000000)
return -ERANGE;
/* Allocate can/net device */
net = alloc_candev(sizeof(struct mcp251x_priv), TX_ECHO_SKB_MAX);
if (!net)
return -ENOMEM;
if (!IS_ERR(clk)) {
ret = clk_prepare_enable(clk);
if (ret)
goto out_free;
}
net->netdev_ops = &mcp251x_netdev_ops;
net->flags |= IFF_ECHO;
priv = netdev_priv(net);
priv->can.bittiming_const = &mcp251x_bittiming_const;
priv->can.do_set_mode = mcp251x_do_set_mode;
priv->can.clock.freq = freq / 2;
priv->can.ctrlmode_supported = CAN_CTRLMODE_3_SAMPLES |
CAN_CTRLMODE_LOOPBACK | CAN_CTRLMODE_LISTENONLY;
if (of_id)
priv->model = (enum mcp251x_model)of_id->data;
else
priv->model = spi_get_device_id(spi)->driver_data;
priv->net = net;
priv->clk = clk;
spi_set_drvdata(spi, priv);
/* Configure the SPI bus */
spi->bits_per_word = 8;
if (mcp251x_is_2510(spi))
spi->max_speed_hz = spi->max_speed_hz ? : 5 * 1000 * 1000;
else
spi->max_speed_hz = spi->max_speed_hz ? : 10 * 1000 * 1000;
ret = spi_setup(spi);
if (ret)
goto out_clk;
priv->power = devm_regulator_get_optional(&spi->dev, "vdd");
priv->transceiver = devm_regulator_get_optional(&spi->dev, "xceiver");
if ((PTR_ERR(priv->power) == -EPROBE_DEFER) ||
(PTR_ERR(priv->transceiver) == -EPROBE_DEFER)) {
ret = -EPROBE_DEFER;
goto out_clk;
}
ret = mcp251x_power_enable(priv->power, 1);
if (ret)
goto out_clk;
priv->spi = spi;
mutex_init(&priv->mcp_lock);
/* If requested, allocate DMA buffers */
if (mcp251x_enable_dma) {
spi->dev.coherent_dma_mask = ~0;
/*
* Minimum coherent DMA allocation is PAGE_SIZE, so allocate
* that much and share it between Tx and Rx DMA buffers.
*/
priv->spi_tx_buf = dmam_alloc_coherent(&spi->dev,
PAGE_SIZE,
&priv->spi_tx_dma,
GFP_DMA);
if (priv->spi_tx_buf) {
priv->spi_rx_buf = (priv->spi_tx_buf + (PAGE_SIZE / 2));
priv->spi_rx_dma = (dma_addr_t)(priv->spi_tx_dma +
(PAGE_SIZE / 2));
} else {
/* Fall back to non-DMA */
mcp251x_enable_dma = 0;
}
}
/* Allocate non-DMA buffers */
if (!mcp251x_enable_dma) {
priv->spi_tx_buf = devm_kzalloc(&spi->dev, SPI_TRANSFER_BUF_LEN,
GFP_KERNEL);
if (!priv->spi_tx_buf) {
ret = -ENOMEM;
goto error_probe;
}
priv->spi_rx_buf = devm_kzalloc(&spi->dev, SPI_TRANSFER_BUF_LEN,
GFP_KERNEL);
if (!priv->spi_rx_buf) {
ret = -ENOMEM;
goto error_probe;
}
}
SET_NETDEV_DEV(net, &spi->dev);
/* Here is OK to not lock the MCP, no one knows about it yet */
ret = mcp251x_hw_probe(spi);
if (ret) {
if (ret == -ENODEV)
dev_err(&spi->dev, "Cannot initialize MCP%x. Wrong wiring?\n", priv->model);
goto error_probe;
}
mcp251x_hw_sleep(spi);
ret = register_candev(net);
if (ret)
goto error_probe;
devm_can_led_init(net);
netdev_info(net, "MCP%x successfully initialized.\n", priv->model);
return 0;
error_probe:
mcp251x_power_enable(priv->power, 0);
out_clk:
if (!IS_ERR(clk))
clk_disable_unprepare(clk);
out_free:
free_candev(net);
dev_err(&spi->dev, "Probe failed, err=%d\n", -ret);
return ret;
}
static int mcp251x_can_remove(struct spi_device *spi)
{
struct mcp251x_priv *priv = spi_get_drvdata(spi);
struct net_device *net = priv->net;
unregister_candev(net);
mcp251x_power_enable(priv->power, 0);
if (!IS_ERR(priv->clk))
clk_disable_unprepare(priv->clk);
free_candev(net);
return 0;
}
static int __maybe_unused mcp251x_can_suspend(struct device *dev)
{
struct spi_device *spi = to_spi_device(dev);
struct mcp251x_priv *priv = spi_get_drvdata(spi);
struct net_device *net = priv->net;
priv->force_quit = 1;
disable_irq(spi->irq);
/*
* Note: at this point neither IST nor workqueues are running.
* open/stop cannot be called anyway so locking is not needed
*/
if (netif_running(net)) {
netif_device_detach(net);
mcp251x_hw_sleep(spi);
mcp251x_power_enable(priv->transceiver, 0);
priv->after_suspend = AFTER_SUSPEND_UP;
} else {
priv->after_suspend = AFTER_SUSPEND_DOWN;
}
if (!IS_ERR_OR_NULL(priv->power)) {
regulator_disable(priv->power);
priv->after_suspend |= AFTER_SUSPEND_POWER;
}
return 0;
}
static int __maybe_unused mcp251x_can_resume(struct device *dev)
{
struct spi_device *spi = to_spi_device(dev);
struct mcp251x_priv *priv = spi_get_drvdata(spi);
if (priv->after_suspend & AFTER_SUSPEND_POWER)
mcp251x_power_enable(priv->power, 1);
if (priv->after_suspend & AFTER_SUSPEND_UP) {
mcp251x_power_enable(priv->transceiver, 1);
queue_work(priv->wq, &priv->restart_work);
} else {
priv->after_suspend = 0;
}
priv->force_quit = 0;
enable_irq(spi->irq);
return 0;
}
static SIMPLE_DEV_PM_OPS(mcp251x_can_pm_ops, mcp251x_can_suspend,
mcp251x_can_resume);
static struct spi_driver mcp251x_can_driver = {
.driver = {
.name = DEVICE_NAME,
.of_match_table = mcp251x_of_match,
.pm = &mcp251x_can_pm_ops,
},
.id_table = mcp251x_id_table,
.probe = mcp251x_can_probe,
.remove = mcp251x_can_remove,
};
module_spi_driver(mcp251x_can_driver);
MODULE_AUTHOR("Chris Elston <celston@katalix.com>, "
"Christian Pellegrin <chripell@evolware.org>");
MODULE_DESCRIPTION("Microchip 251x/25625 CAN driver");
MODULE_LICENSE("GPL v2");
安卓的驱动能不能参考其他家的IC代码修改一下,只改寄存器相关的内容?
理解您的意思,但是这个我们没有实际验证过呢。
另外CAN相关的调试工具有吗?比如canutils或者其它.
很抱歉也没有呢。