This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear sirs,
我司目前收到車廠RFQ
其車機端是使用DS90UB681 .請問RX 端應該搭配TI哪一款 IC
在請提供資訊
謝謝
Dear Sirs,
Our company currently receives RFQ
The vehicle side uses DS90UB681. Which RX IC should be paired to this TX
Please provide information
Thanks
您好,681可以和ADAs系列的936, 954, 960, 962, 9702, 9722搭配使用。
也可以92x以及分辨率达到1080p的94x搭配使用,都是可以的。
所以您选择DS90UH928Q是可以和681搭配使用的。
抱歉,DS90UB681是NDA器件,无法直接给您提供,并且官网没有给出直接申请的链接。
是需要客户进行申请的。贵公司是否有和TI直接对接的FAE联系?如果需要申请的话,可以联系他们。
或者需要我这边帮忙的也可以随时讨论。