Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: DS90UB960-Q1
一个客户车载环视主机是960,摄像头采用935配置参数。
但是由于960的解串板买不到,生产车间生产调试的工装买了954的解串板,客户想了解,能否直接用954来做监视器调试呢?以前的和960匹配好的参数还需要重新调整么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: DS90UB960-Q1
一个客户车载环视主机是960,摄像头采用935配置参数。
但是由于960的解串板买不到,生产车间生产调试的工装买了954的解串板,客户想了解,能否直接用954来做监视器调试呢?以前的和960匹配好的参数还需要重新调整么?
您好,通过对比954和960的数据手册,差异如下:
DS90UB954-Q1:
-Dual deserializer hub that is capable of aggregating data from up to two sensors using two separate FPD-Link III interfaces
-One MIPI CSI-2 Output Port (Supports 1, 2, 3, and 4 Data Lanes per CSI-2 port)
-One I2C port that can support up to 1 Mbps (Fast-Mode Plus)
DS90UB960-Q1:
-Quad deserializer hub that is capable of aggregating data from up to four sensors using four separate FPD-Link III interfaces
-Two MIPI CSI-2 Output Ports (Supports 1, 2, 3, and 4 Data Lanes per CSI-2 port)
-Two I2C ports that can support up to 1 Mbps (Fast-Mode Plus)
那关于寄存器配置的对比,还是要对比下二者的数据手册的register map。
按照这个原理图,参数如何配置呢,如何配置寄存器?
您好,我不知道您指的哪些参数。通过硬件电路主要是看MODE引脚的配置,或者是可以通过寄存器的配置将硬件配置覆盖掉。
在您的电路中,MODE上拉R61=10K和下拉R63=10Kohm电阻,根据Table7-9 MODE的配置,只有下拉10K代表的是sync同步模式。您是需要同步模式吗?
根据这个表格,在不同模式下,MODE引脚选择不同的上下拉阻值,如下。

如果实际应用中,发现MODE引脚配置不是想要的模式,也是可以通过0x04 bit4 MODE_OV=1,即为寄存器的配置覆盖MODE引脚的配置。
感谢您的支持,客户确实是选择的Mode0同步模式,实际上电路上的R61/R62是空贴状态,我们现在需要对935做初始化的寄存器配置,这部分的配置参数烦请您支持提供一下。客户表示这部分行业里都是TI提供的配置
抱歉这些FPD link器件没有初始化配置可以提供呢,因为只要硬件MODE_SEL配置正确,不需要配置或者初始化都是可以工作的。