This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4551-Q1: 请问芯片支持的CAN FD的最高速率到底是8Mbps,还是5Mbps?

Part Number: TCAN4551-Q1

在芯片DataSheet的首页描述内容是: Supports CAN FD data rates up to 8 Mbps with up to 18 MHz SPI clock speed

但是在芯片DataSheet的第20页(8.1 Overview)的描述内容是: The TCAN4551-Q1 is a CAN FD controller with an integrated CAN FD transceiver supporting data rates up to 8 Mbps. The CAN FD controller meets the specifications of the ISO 11898-1:2015 high speed Controller Area Network (CAN) data link layer and meets the physical layer requirements of the ISO 11898-2:2016 High Speed Controller Area Network (CAN) specification providing an interface between the CAN bus and the CAN protocol controller supporting both classical CAN and CAN FD up to 5 megabits per second (Mbps).

  • 您好,

    该设备支持的最高速率是8 Mbps。上面提到的 5 Mbps 是ISO 11898 -2物理层标准中定义的最大数据速率。虽然 8Mbps 时序参数未通过ISO标准,但TCAN4551可以以此速率工作。因此如果客户的应用需要更快的速度,并且可以脱离现有的11898 -2物理层定义,则可以使用这种更高的操作速度。另外注意系统可实现的最大速率是由整个网络的工作条件决定的,而不是取决于TCAN4551这一个器件。