Part Number: TCAN4550-Q1
条件:
车上CAN总线有一百多个ID,当有新的消息存进RX FIFI 0的时候,掉用TCAN4x5x_MCAN_ReadNextFIFO读取数据,读回来的MsgHeader.ID和dataPayload的数可能会对应不上,也就是收到MsgHeader.ID是ID(A),但是dataPayload可能是data(B)或者其他ID的数据,我想尝试用过滤ID的方法解决这个问题,但是过滤器没起作用,我任然能收到CAN总线上的所有ID。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN4550-Q1
条件:
车上CAN总线有一百多个ID,当有新的消息存进RX FIFI 0的时候,掉用TCAN4x5x_MCAN_ReadNextFIFO读取数据,读回来的MsgHeader.ID和dataPayload的数可能会对应不上,也就是收到MsgHeader.ID是ID(A),但是dataPayload可能是data(B)或者其他ID的数据,我想尝试用过滤ID的方法解决这个问题,但是过滤器没起作用,我任然能收到CAN总线上的所有ID。
您好,您的这个问题周五我已经提交到英文E2E上了,暂时还没得到回复,请关注E2E的回复,一旦回复了有任何问题您都可以直接在上面跟进:
您好,您的这个问题E2E已经给出回复:需要您提供一些寄存器的值以便帮助分析,包括实际的信息头文件, message header, data payloads, 以及 filter elements 。
Please provide the register values they are using for the device as well as the actual message header, data payloads, and filter elements they are using so that I can check them for errors. I unfortunately can't help without actual detailed register data and the actual message header ID information.
感谢回复,该问题已经解决。将全局滤波器设置寄存器0x1080中的ANFS和ANFE都设置为2,就可以过滤出想要的ID和数据,读回来的数据也不会错乱了。