在使用SN75DP159时,一开始使用的是I2C配置模式,可以正常使用。后面选用PIN STRAP模式,但始终无法正常使用,有HPD给到源,但DDC测量不到信号,源输入也没有,但是这时用i2c还是可以读写寄存器,然后正常输出图像。想请专家帮忙分析原因并看下我的原理图设计有没有问题。04-HDMI_TX1.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用SN75DP159时,一开始使用的是I2C配置模式,可以正常使用。后面选用PIN STRAP模式,但始终无法正常使用,有HPD给到源,但DDC测量不到信号,源输入也没有,但是这时用i2c还是可以读写寄存器,然后正常输出图像。想请专家帮忙分析原因并看下我的原理图设计有没有问题。04-HDMI_TX1.pdf
没有了,就通过I2C_EN脚:

DP159 and DP149 Configuration Guide
看下面checklist ,I2C 信号通过1k电阻下拉,不知道是不是这个原因造成的,您尝试修改下这里看是否可以进入PIN STRAP模式