This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: DS90UB954----DS90UB933 LINK上,但954无信号输出

Part Number: DS90UB954-Q1

Dear TI:

 1、问题描述:

   目的: 适配带串化器为UB933的摄像头(解串器为UB954-Q1);

    按照附件图1配置初始化954-933寄存器后,发现ub933-UB954能够LINK上,但查看0X4D寄存器,该寄存器值始终为0x03(即无信号输入给到  

   ub954),另外ub954 0x73-0x76 寄存器值保持不变,且摄像头无法出图

2、问题现象:

    按照附件图1配置初始化UB954-UB933后,ub954无信号输出(绝大部分时间),但偶尔能出现信号(复现手法:重新reset ub954,重新初始化933-954,出图为一帧灰色叠层图,出图后即卡住,不能连续出图,如附件图2所示)

 3、硬件环境:

    硬件原理图如附件图3所示,摄像头参数如附件图4所示;

    连接方式:soc主控-----DS90UB954----DS90UB933 -------senosr(摄像头sensor)

 4、期待结果:

   954-933寄存器信号能够正常通信,且图像正常;

5、疑问点

      ①场帧内同步和外同步有啥区别?  什么时候该用内同步什么时候该用外同步?

      ②ub954 设置寄存器0x58,为i2c_pass_through后 ,是否ub933-ub954Link上,是否可以通过查看0X5b寄存器是否为slave i2c address判断?

6、附件:

    附件图1:UB954-933在soc的初始化配置;

    附件图2:问题现象图;

    附件图3:摄像头与ub954连接原理图;

    附件图4:适配的摄像头参数(带串化器UB933);

    附件图5:ub954-933 soc系统dump数据;

u954问题附件.zip

期待能够得到解答,非常感谢!

x 出现错误。请重试或与管理员联系。