This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于SN74LVC245A工作电压范围问题

Other Parts Discussed in Thread: SN74LVC245A

查阅TI官网上SN74LVC245A器件的datasheet,VCC工作电压范围为1.65~3.6V。该器件可以工作在3.3V电压下。
但是Absolutely Maxium Ratings一项中VCC的最大最小值为-0.5~6.5V,这两个范围应该如何理解?
该芯片是否可以工作在5V VCC电压? 如果强制让该芯片工作在5V电压下,会有什么影响?谢谢解答。

  • VCC工作电压范围为1.65~3.6V,这个是可以保证正常工作的范围,超过这个范围,比如用5V供电,其各项电气参数不能得到保证。-0.5~6.5V这个范围指的是芯片可以承受的绝对最大范围,超过则会损坏芯片

  • 芯片的功能性测试还是参考datasheet中“RECOMMENDED OPERATING CONDITIONS”的电气特性,所以在使用任何一款器件时,都参考推荐值,也就是说对于这款来说,工作电压范围为1.65V~3.6V,是不允许5V供电的。

    而Absolutely Maxium Ratings在datasheet中也有注释:Stresses beyond those listed under Absolute Maximum Ratings may cause permanent damage to the device. These are stress ratings only, and functional operation of the device at these or any other conditions beyond those indicated under Recommended Operating Conditions is not implied. Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability.这个只是压力测试,如果按照这个范围使用,会损坏器件的。

  •  如果强制让该芯片工作在5V电压下,会有什么影响? ---------- 在这个条件下,生产商不能保证芯片能够正常工作。

  • 这个和我的理解是一样的,谢谢解答。