This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB983 设计相关问题

TI team,您好

目前在设计一个4k分辨率图片显示的项目,需使用到DS90UB983,关于手册中Typical Application部分这边有几个问题相咨询一下:

1. VDD11供电为何给的是1.15V而不是1.1V? 我看大多数设计都是1.1V啊

2. 关于链路上的AC耦合电容为何由0402封装改成0201,有什么好处或者影响吗

3. 关于使用的CMC及ESD这边有推荐使用的型号吗(CMC使用这个ACM1211-102-2PL-TL-01,ESD使用PESD5V0S1BA 可以吗)

4. 983上面有3个IIC,使用一个可以吗,什么情况下同时用三个