This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550: 为什么TCAN4550的SPI SDO没有响应数据?

Part Number: TCAN4550


1、与TCAN4550通信的DEMO工程是我之前的工程,已经能够与TCAN4550的DEMO板能够正常通信,即:我的M3可以通过4550转的CAN,与外部CAN进行双向通信。

2、把同样的工程拉出来,与我的控制板(还是M3与TCAN4550通过SPI通信,4550转换CAN),,问题是:给TCAN4550发送的时序看起来没有问题,如下图所示:

上图中CH4:CS; CH1:SCK;CH3:M3的MOSI,CH2:M3的MISO(也就是TCAN4550的输出)

3、检查我的复位上电时序,如下图所示:

上图中CH4:CS; CH1:SCK;CH3:M3的MOSI,CH2:TCAN4550的RST(现在是通过M3的IO来控制的);

4、检查了一下TCAN4550的各管脚电平,如下图所示:

5、测量了一下我的SPI时钟,900KHz,小于1MHz;

排查了以上因素外,,TCAN4550还是没有SPI通信口的SDO输出信号,,请问,,哪里还存在问题,引起TCAN4550的SPI(SDO 6脚)没有响应数据?

期待回复!