Part Number: TMDS181
Other Parts Discussed in Thread: TUSB3410
看TMDS181的数据手册说,可以进行PRBS测试,然后通过I2C导出数据,那导出数据后怎么去分析,判断信号质量的好坏,是要转换成眼图来看吗?还有DP159也是一样的做法吗

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,TMDS181/171在每个TX lane与pattern generator,这些pattern支持很多标准的PRBS 时序可以使用,可以参考这篇应用手册里面给出了如何去写I2C的寄存器配置:
https://www.ti.com/lit/ug/sllu294/sllu294.pdf
您看下这个帖子和您的问题类似,您可以参考下:
是的,通过这个Debug tool对导出的数据绘制成眼图进行分析。
我了解到要用TUSB3410 EVM配合EyeScan 软件才能看到眼图,现在TUSB3410 EVM申购不到,还有其他工具可以使用吗,或者其他的USB转IIC工具(不是USB3410芯片)适用吗。谢谢!
您好,我看了下EyeScan Tool确实需要类似TUSB3410这种将USB转I2C的器件来搭配使用,但是目前除了TUSB3410,没有其他桥接芯片可以实现USB转I2C呢。