This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9535: 芯片的应用问题

Part Number: PCA9535


pca9535A的gpio被拉低导致i2c异常

扩展芯片的P6被拉低了导致i2c异常

同样的设计没有做任何设计变化,之前客户反馈老的批次的料没问题,新换的这批料有这个问题,io扩展芯片初始化也是失败的.

现在我们临时把R23去掉解决这个问题的

帮忙看看可能哪里有问题并给出解决办法,谢谢!

  • 您好,看下内部简单架构,IO要么为高电平(Q1导通,Q2关闭)。要么为低电平(Q1关闭,Q2导通)。您现在遇到的问题是P06 port被拉低导致I2C异常。

    有做什么动作导致被拉低了吗?之前都是正常工作的?

    另外R23这里是0ohm电阻吗?去掉R23能解决的意思,是断开R23这里吗,相当于和U1断开吗?但是您上面也提到去掉U1同样问题复现,所以不太理解您这里的意思。