This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello, the attached schematic is unclear even though I amplifier it, you could refer to the schematic checklist for reference:
https://www.ti.com.cn/cn/lit/an/slla481/slla481.pdf
If you have any other questions, please follow up directly.
Please refer to the schematic checklist, if you have any doubts about which pins, we could discuss each other.
Hi Kailyn,
In the application circuit of the TUSB321 datasheet (Page14), why do TUSB321 CC1&CC2 pin need to be reversed?
Similarly, the polarity of HD3SS321 C0P/C0N & C1P/C1N circuit is also reversed.
Is there any special purpose for this?
If it possible if I don't reverse the polarity of the above pins?
您好,我们直接用中文沟通吧。
首先CC1和CC2 是可以交换的,另外HD3SS3212的差分信号的P和N的极性都是可以交换的,因为layout的原因有时按照PN的顺序无法布线,所以会将PN极性颠倒一下,只要保证凯开关的发送和接收端的PN极性一致即可。