This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS160PR1601: 是否支持PCIe Gen 1.0和PCIe Gen 2.0

Part Number: DS160PR1601

Hello experts!

 我看手册里面写明确支持PCIe Gen 3.0和PCIe Gen 4.0的应用,这里对PCIe Gen 1.0和PCIe Gen 2.0有个note,我想知道这个芯片是否可以向下兼容PCIe Gen 1.0和PCIe Gen 2.0的应用呢?

 

thanks!

  • 如果不能支持,是否有可以兼容PCIe Gen1.0到PCIe Gen 4.0的合适中继器推荐,十分感谢!

  • 您好,通常我们在使用能支持更高协议的器件时,对于协议的最初spec都是可以向下兼容的,但是对于DS160PR1601来说,它能支持到PCIE GEN3或gen4,甚至有些redriver能支持到GEN5,使用它应用在gen1或2上,那么gen1或2的损耗预算会相比gen3或4更大。

    数据手册中提到“no link training for PCIE gen1 and 2”是因为PCIE gen2是十几年前的规范了,那么PCIE Gen1会更早,针对gen1和2,没有参考电路也没有实际去做验证。

  • 您好,这里损耗指的是插损吗?我理解是频率越低插损越小,这里的更大指什么呢?谢谢~

  • 同频条件下,应用于PCIE GEN1&2条件下可能会比GEN3&4条件下的均衡能力弱一些,或者说我们使用redriver 目的是为了补偿高频和低频信号的衰减差, 那这种补偿能力可能会没有GEN3&4要强一些。可以向下兼容,但是可能达不到GEN3和GEN4高速率条件下的性能,有点儿大材小用。

  • Hi Kailyn,

    还有如下两个问题,麻烦帮忙确认下,谢谢!

    1.我们使用场景要兼容PCIe Gen1.0到PCIe Gen 4.0,有没有SI的模型可以提供?

    2.调试时需要看眼图,需要用到Sigcon Architect的软件,可否帮忙批一下,好像需要申请,保证能够支持 DS160PR1601。

  • 我们使用场景要兼容PCIe Gen1.0到PCIe Gen 4.0,有没有SI的模型可以提供?

    抱歉没有SI model。

    调试时需要看眼图,需要用到Sigcon Architect的软件,可否帮忙批一下,好像需要申请,保证能够支持 DS160PR1601。

    您好,需要自行申请,提交到美国那边的哈,并且申请的时候使用英文填写信息。