This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通过寄存器可以修改的是Vod的输出幅值,默认的是-0.4dB,570mV,但是可以通过寄存器配置修改Vod。驱动走线这里没有寄存器可以表明走多长线对应Vod的大小。
只能在layout时尽量控制在1~2inches内。
另外, Programming Guide是需要自行申请的,抱歉我这边无法发给您。
给您带来不便非常抱歉。
有的,对于我6G和12G速率来说,寄存器0x03默认值为0x80, PCB FR4 的trace,可以驱动10~15inch的长度。
另外也有一个这样的表格,给出了3G和6G速率下boost setting以及trace的长度。
建议您申请下这个programming guide,帮助您design。