This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1145-Q1: CAN芯片短路测试烧坏

Part Number: TCAN1145-Q1
Other Parts Discussed in Thread: TCAN1146-Q1, TCAN1144-Q1

TCAN1145-Q1的CAN总线短路到电源,器件烧坏,同样的测试条件TCAN1042正常,TCAN1145-Q1没有短路保护功能么

  • 您好,

    是的,TCAN1145-Q1没有短路保护功能。

    datasheet 中 10.4.8 Bus Fault Detection and Communication (TCAN1144-Q1 and TCAN1146-Q1),都是针对TCAN1144-Q1 and TCAN1146-Q1这两个器件的描述。

  • 数据手册上写的CANH和CANL能承受58V呀,现在是TCAN1145不能承受58V吗?这样的话TCAN1145具体能承受多少V呢?

  • 数据手册上写的CANH和CANL能承受58V呀,现在是TCAN1145不能承受58V吗?这样的话TCAN1145具体能承受多少V呢?

  • 看绝对最大额定值表格,CANH和CANL 最大耐压±58V。你是使用58V电压测试的CANH和CANL对地耐压吗?具体你是怎样测试的?我担心在上电瞬间电压有浪涌超出了58V或电压不稳而损坏设备。

  • 我们是单独CANH或CANL加一个33V(对GND)电源。然后和芯片同时上电。就烧坏了,还远没到58V。我们的电源是专业的设备,应该不会产生太大的浪涌。另外我们使用同样的测试方法测试别的品牌的CAN芯片是没有问题的。

  • CAN芯片先上电,然后CANH/CANL再接到32V也测过,同样会烧坏。

  • 这个不应该损坏,在绝对最大额定值表格里CANH/CANL最大耐压±58V。建议你确认下所测试芯片购货最终来源是否为TI,如果确认购货来源是TI,建议您将问题发布在E2E英文技术论坛上,问下资深的英文论坛工程师是什么原因,英文论坛对应子论坛链接:

    https://e2e.ti.com/support/interface-group/interface/f/interface-forum