Part Number: DP83848I
Hello,在DP83848I的设计中,目前我们设计中发现,需要使用外同步时钟。请帮忙确认下如下几点:
1.RMII 工作在Master Mode还是Slave Mode,还是两者均可?如果均可,如何去修改配置?
2.RMII 如果工作在Slave Mode,50M的时钟BUFFER的等长需要如何处理?TX和RX的Data/Control 均需要相对于REF_CLK做等长么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83848I
Hello,在DP83848I的设计中,目前我们设计中发现,需要使用外同步时钟。请帮忙确认下如下几点:
1.RMII 工作在Master Mode还是Slave Mode,还是两者均可?如果均可,如何去修改配置?
2.RMII 如果工作在Slave Mode,50M的时钟BUFFER的等长需要如何处理?TX和RX的Data/Control 均需要相对于REF_CLK做等长么?
您好,
首先回答您的第一个问题,因为这个料是物理层的PHY收发器,对于物理层来讲,Master Mode还是Slave Mode主要是数据方向不同,这个料是双向的,而且你看datasheet的内部框图,有个Auto-MDIX模块,自动切换数据收还是发的方向。所以我的理解,Master Mode还是Slave Mode应该都是可以的。只需要配置Auto-MDIX enable就可以。
正常是默认enable的,(Auto-MDIX is enabled by default and can be configured through strap or through PHYCR (19h) register, bits [15:14].)
关于第二个问题,肯定是建议等长的,TX,RX和CLK等时序信号之间建议是等长的。
datasheet中也有相关的建议:
It is recommended to keep the signal trace lengths as short as possible. Ideally, keep the traces under 6 inches. Trace length matching, to within 2.0 inches on the MII or RMII bus is also recommended.
希望回答对您有帮助。
关于REF CLK,您可以看一下这个文档:https://www.ti.com/lit/an/snla076a/snla076a.pdf?ts=1712628477236
page3,有关于这个时钟的描述,可以使用外部时钟。
REF_CLK is an input to the DP83848 and may be sourced by the MAC or from an external source such as a clock distribution device
RMII的工作模式,我是这样理解的,如果说Mac层的master和slave模式,肯定是不同的,包括数据处理机制,但是物理层PHY这块,是不需要考虑数据传输机制的,只需要考虑信号的转换,方向,电平等,所以我理解两种模式都是可以的,我们也可以继续探讨这个话题。