你好,我们使用DP83TC812S-Q1芯片,现在无法进入test mode,
步骤如下:
0x1836的bit[13-15]写入对应的值,然后读出来的值一直是0
还需要做什么其他操作吗?操作其他的寄存器,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我们使用DP83TC812S-Q1芯片,现在无法进入test mode,
步骤如下:
0x1836的bit[13-15]写入对应的值,然后读出来的值一直是0
还需要做什么其他操作吗?操作其他的寄存器,谢谢
您好,
请参考链接网页上芯片驱动“ LINUX-DP83TC812” : ETHERNET-SW Driver or library | TI.com
数据手册https://www.ti.com/lit/ds/symlink/dp83tc812s-q1.pdf
“8.6.1 Register Access Summary”说明了寄存器地址接口,0x1836属于MMD1 field。
"8.4.18.1" 和“8.4.20.1”列出了写入寄存器的具体步骤。
读取0x1836寄存器,请参考“Table 8-26” 中“MMD1 Field” 步骤。
您好,
DP83TC812S-Q1是百兆PHY, 不支持千兆。
“The DP83TC812S-Q1 is a 100BASE-T1 automotive Ethernet Physical Layer transceiver.”