Part Number: TCAN4550
TCAN4550 使用中断接收数据,配置通过GPIO1引脚触发;
目前测试接收数据在帧间隔小于5ms时,丢包比较严重;
想请问下,TCAN4550芯片稳定收发数据最短帧间隔可以到多少;
如果是帧间隔小于1ms可以稳定收发,那么是否是我的配置问题,需要怎么检查;
期待回复!
下图是两组测试数据,左图:帧间隔5ms1000帧数据丢包率0.1%,右图:帧间隔1ms1000帧数据丢包率19.6%。


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.