我们使用在 intel soc 和ec之间做电平转换,intel这边是1.8伏的, ec这边是3.3伏的,intel soc 高电平输入要求 是最小0.8X 1.8V,而现在只是知道txb0304高电平输出的最大值是0.9 x vcci,无法确定其最小高电平出值,在这边是没有上下拉电阻的,怎样可以确保电平的正确触发?在ec这边有一个有10K欧姆的上拉电阻,有一个没有上拉电阻,是不是有上拉电阻后,其输出的低电平的最大电压为0.43伏?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们使用在 intel soc 和ec之间做电平转换,intel这边是1.8伏的, ec这边是3.3伏的,intel soc 高电平输入要求 是最小0.8X 1.8V,而现在只是知道txb0304高电平输出的最大值是0.9 x vcci,无法确定其最小高电平出值,在这边是没有上下拉电阻的,怎样可以确保电平的正确触发?在ec这边有一个有10K欧姆的上拉电阻,有一个没有上拉电阻,是不是有上拉电阻后,其输出的低电平的最大电压为0.43伏?谢谢!
要看具体你是几V到几V的电平转换,比如你这里是1.8V到3.3V的转换,那么就按照3.3V 电平的门限,Voh(min)=2.4V,Vol(max)=0.4V。