This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8041: 热插拔上行端口,不能识别下行USB3.0接口

Part Number: TUSB8041


1,PC与hub之间插入USB3.0线缆,然后再上电,能够正常识别下行端口的USB3.0设备。然后插拔上行端口的USB3.0设备,就无法识别下行端口的USB3.0设备。

2,USB2.0设备上电和插拔正常

3,在上电识别到下行USB3.0的情况下,插拔下行端口的USB.0设备,可以正常识别。

4,在1的基础上,插拔下行USB3.0设备,可以正常识别。

5,有的设备全部正常,有的设备会出现这个问题。

注:设备由外部电源供电,hub的3.3V比1.1V上电提前1.68ms,GRST比3.3V延迟14ms抬高。

上行输入TYPEc接口原理图

typec接口转到HUB的上行端口

hub原理图

下行端口原理图