This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM26LV31: 芯片VOD的值的问题

Part Number: AM26LV31

你好,请问关于AM26LV31的问题。

我的后端伺服控制的差分输入需要VT值2.5~3.8V之间,

1)请问这款芯片的差分输出电压能否满足。我确认了datasheet,好像只有1.5V?

2)这款芯片是3.3V供电的,同样的AM26LV31E也是3.3V的,感觉后者的VOD要大很多,为什么?

3)我测试了我测试基板上的AM26LV31IDR的输出,使用差分探头测量的差分电压其实是有3V. 和datasheet上的内容是不是有不同点,为什么?我测试是否不准确?

谢谢