典型参考原理设计中,8、9、11、12引脚的差分对接到HOST端的TX、RX通道。19、20、22、23引脚的差分对连接到device端的RX、TX通道。
该设计是否支持HOST、device端角色互换?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
感谢您对TI产品的关注!图中Host和Receptacle的位置是可以互换的。可以参考下面帖子:
"you can swap which side of the device will connect to the USB host or Receptacle"
TUSB522PEVM评估模块使用的也是这种连接方式,您可以对照参考下EVM用户指南和TUSB522PEVM页面里的设计文件进行设计:
TUSB522PEVM用户指南
TUSB522PEVM页面里面有设计文件
为更加有效地解决您的问题,建议您按照更改TI账户邮箱地址.pdf将邮箱更改为公司邮箱,然后在美国E2E上发帖 https://e2e.ti.com/,将由资深的英文论坛工程师为您提供帮助。