This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125DF1610EVM: VOD设置

Part Number: DS125DF1610EVM


您好,我想问两个问题。

1.每个通道的 VOD电平都可单独设置吗?

2.如果将一个通道的输入广播到另外三个频道,现在这4个通道的VOD也可单独设置是吗?

谢谢。

  • 您好,

          1)可以。请参考“Table 6. Typical VOD Settings” + “channel registers”。

          

         2)可以。通道广播使用的CrossPoint是输入路径,用于VOD设置的driver模块是输出路径,不影响。

               具体请参考数据手册“Figure 1” 和“Figure 2”。