Hi:
In the reference design, TVS CDSOT23-SM712 was used to suppress 1kV inrush current and passed the test. Who knows what the surge current is during the surge test? The picture shows the circuit being tested in the reference design.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi:
In the reference design, TVS CDSOT23-SM712 was used to suppress 1kV inrush current and passed the test. Who knows what the surge current is during the surge test? The picture shows the circuit being tested in the reference design.

Hello:
Thank you for answering my question.
It seems that 10/700μs combined wave transmitter is used here for surge test, but for CDSOT23-SM712 component, its maximum surge current is 17A (in the case of 8/20μs), if the surge current is 25A, Then the maximum peak current that TVS needs to withstand (in the case of 8/20μs) is about 25×17.5=437.5A (according to theory, 10/350μs and 8/20μs under the same lightning current, the ratio of 10/350μs and 8/20μs lightning joule energy is 17.5:1), Obviously, it far exceeds the current that CDSOT23-SM712 can withstand, but why can it also withstand 1kV surges?
The picture shows the electrical parameters of CDSOT23-SM712.

为更加有效地解决您的问题, 建议您按照5238.更改TI账户邮箱地址.pdf将邮箱更改为公司邮箱,然后在美国E2E上发帖重新问下这个问题 e2e.ti.com/,将由更专业的资深英文论坛工程师为您提供帮助。