This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550-Q1: SPI通信SDO无响应

Part Number: TCAN4550-Q1


我现在调试TCAN4550-Q1芯片,SDO没有反应。
我查看了一下SCLK,SDI,CS波形是对的,INH没有电压,VCCOUT有5V电压,我怀疑过是芯片进入了睡眠模式,但是尝试了翻转RST,重新上电没有作用。
我也怀疑是晶振有问题,尝试读取寄存器0x0000,0x0004也没有回应,VSUP电压+12V,VIO电压+3.3V。
请问还有什么情况下会出现SDO没有反应的情况。

谢谢

  • 另外SPI模式我选择的是MODE 0(CPOL=0,CPHA =1),因为我看论坛里模式大部分是这样的,但是我看数据手册里是MODE 0(CPOL=0,CPHA =0),请问那一个是正确的,两个模式我都尝试了一下都没有成功收到SDO的回传数据