Other Parts Discussed in Thread: TUSB1046-DCI, TUSB546-DCI
我们需要用type-c接口走dp信号传输视频,4lan模式,单lan速率到8Gbps。目前从官网上看到有TMUXHS4446,TUSB1046,TUSB546这三个型号似乎都可以,不知道这三个型号有什么区别??能否推荐一下我们走dp信号的场景用哪个型号合适呢??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们需要用type-c接口走dp信号传输视频,4lan模式,单lan速率到8Gbps。目前从官网上看到有TMUXHS4446,TUSB1046,TUSB546这三个型号似乎都可以,不知道这三个型号有什么区别??能否推荐一下我们走dp信号的场景用哪个型号合适呢??
您好,
TMUXHS4446支持 DisplayPort 2.1,单Lane速率可以达到10Gbps,而另外两个型号是支持DisplayPort 1.4,而且TUSB546-DCI的USB 3.1速率为5Gbps,这可能对于某些需要更高USB速率的应用来说是不够的。TMUXHS4446和TUSB1046-DCI都完全适合您的应用需求。如果您对USB速率有更高的要求,建议选择TMUXHS4446;如果USB速率不是主要关注点,那么TUSB1046-DCI也是一个很好的选择。