This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ds80pci402延长眼图问题上位机不能侦测到device

Other Parts Discussed in Thread: DS80PCI402

使用TI ds80pci402延长pcie信号,上位机台式机不能侦测到device,先给建议:

线缆是定制的。

ds80pci402测试现象

1 连接关系

                       

1)        PC:PCIE1.1主设备,重启时自动枚举PCIE设备

2)        PCIE Adapter:一段连接PCIE延长线,另一端通过金手指与主机连接,具有负载均衡功能,负载均衡功能由ds80pci402实现,可通过拨码开关对预加重值和均衡值进行调节

3)        PCIE Cable:Manufacture is one stop systems,and one stop systems use molex products.

4)        device:PCIE1.1从设备,使用xilinx公司的XC7A100T-2FGG484C实现PCIE协议,使用TI公司的ds80pci402实现PCIE信号负载均衡

2 核心器件表

序号

器件名称

器件用途

位置

参考文档

1

XC7A100T-2FGG484C

实现PCIE协议

device

《ug475_7Series_Pkg_Pinout》

2

ds80pci402

实现负载均衡

PCIE Adapter/device

《ds80pci402》

3

smt主连接器(75586-0011)

Connect component on device and PCIE Adapter

PCIE Adapter/device

《PS-75586-001》

4

emi导向框(74540-0401)

Connect component on device and PCIE Adapter

PCIE Adapter/device

《0745400401_IO_CONNECTORS》

5

CABLE-PCIe-x4-3M

PCIE延长线

PCIE Cable

 

 

3 现象

1)        信号眼图不理想

  • 在device能够检测到pc发送的CLOCK信号,连接关系如下图蓝色箭头所示,眼图参见PCIE_CLOCK(100MHz).jpg。时钟信号没有经过ds80pci402。
  • device向PC不停发送PCIE信号,在四个测试点抓取差分信号,如下如黄色箭头所示,眼图参见eye_diagrams_1.jpg、eye_diagrams_2.jpg、eye_diagrams_3.jpg、eye_diagrams_4.jpg

 

2)        device的ds80pci402寄存器值与预期不符

  • 如下图蓝色箭头所示,给ds80pci402的寄存器赋初始值;然后重启PC,PC枚举PCIE设备;PC枚举结束后,读取device中的ds80pci402寄存器值,测试情况如下表所示

Address

Register   Name

Initial   Value

Read   Value

Expect   Value

0x0E

CH0-CHB0   IDLE, RXDET

0x08

0x08

0x08

0x11

CH0-CHB0-DEM

0x02

0x02

0x82

0x15

CH1-CHB1   IDLE, RXDET

0x08

0x08

0x08

0x18

CH1-CHB1-DEM

0x02

0x02

0x82

0x1C

CH2-CHB2   IDLE, RXDET

0x08

0x08

0x08

0x1F

CH2-CHB2-DEM

0x02

0x02

0x82

0x23

CH3-CHB3   IDLE, RXDET

0x08

0x08

0x08

0x26

CH3-CHB3-DEM

0x02

0x02

0x82

0x2B

CH4-CHA0   IDLE, RXDET

0x08

0x08

0x08

0x2E

CH4-CHA0-DEM

0x02

0x82

0x02

0x32

CH5-CHA1   IDLE, RXDET

0x08

0x08

0x08

0x35

CH5-CHA1-DEM

0x02

0x82

0x02

0x39

CH6-CHA2   IDLE, RXDET

0x08

0x08

0x08

0x3C

CH6-CHA2-DEM

0x02

0x82

0x02

0x40

CH7-CHA3   IDLE, RXDET

0x08

0x08

0x08

0x43

CH7-CHA3-DEM

0x02

0x82

0x02

 

  • 如下图黄色箭头所示,给ds80pci402的寄存器赋初始值;然后device的XC7A100T-2FGG484C向PC发送信号;信号发送一段时间,大概5至7秒,读取device中的ds80pci402寄存器值,测试情况如下表所示

Address

Register   Name

Initial   Value

Read   Value

Expect   Value

0x0E

CH0-CHB0   IDLE, RXDET

0x08

0x08

0x08

0x11

CH0-CHB0-DEM

0x02

0x82

0x02

0x15

CH1-CHB1   IDLE, RXDET

0x08

0x08

0x08

0x18

CH1-CHB1-DEM

0x02

0x82

0x02

0x1C

CH2-CHB2   IDLE, RXDET

0x08

0x08

0x08

0x1F

CH2-CHB2-DEM

0x02

0x82

0x02

0x23

CH3-CHB3   IDLE, RXDET

0x08

0x08

0x08

0x26

CH3-CHB3-DEM

0x02

0x82

0x02

0x2B

CH4-CHA0   IDLE, RXDET

0x08

0x08

0x08

0x2E

CH4-CHA0-DEM

0x02

0x02

0x82

0x32

CH5-CHA1   IDLE, RXDET

0x08

0x08

0x08

0x35

CH5-CHA1-DEM

0x02

0x02

0x82

0x39

CH6-CHA2   IDLE, RXDET

0x08

0x08

0x08

0x3C

CH6-CHA2-DEM

0x02

0x02

0x82

0x40

CH7-CHA3   IDLE, RXDET

0x08

0x08

0x08

0x43

CH7-CHA3-DEM

0x02

0x02

0x82

 

4 reference

1)        schematic.pdf

2)        device pcb layout.png

3)        pg054-7series-pcie (1).pdf

4)        ds80pci402

5)        0745400401_IO_CONNECTORS.pdf

6)        PS-75586-001.pdf

7)        eye_diagrams_1.jpg

8)        eye_diagrams_2.jpg

9)        eye_diagrams_3.jpg

10)    eye_diagrams_4.jpg

11)    PCIE_CLOCK(100MHz).jpg

 

TO TIFAE.rar
  • Hi Viking,

    请问这个问题的最新状态是什么样的?

    1. 我查了原理图, 没有看到问题

    2. 寄存器配置,你这边有没有把寄存器6的bit3写成 ‘1’? 这样寄存器0x06的值是0x18。 这样设置以后寄存器配置才会生效。

    3. 关于你写的值和读出来不一样,比如寄存器0x11, 它的最高为是RXDET的状态位,是只读的。因为你设置了原理图上rxdet=1,这个bit会变成'1'

    如果你这边还有问题,请告知我最新的情况。

    Regards,

    Liang

    Regards

    Liang