This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB925Q与DS90UB928Q配对使用时传导发射的问题



请教下论坛里的工程师们: 使用了一对DS90UB925及DS90UB928的LVDS芯片来实现视频信号的传输,两个IC分别位于两个设备上,用LVDS 双绞线实现传输,在928的输入处加一个共模电感。目前在EMC测试时发现CE电流法超标。超标点约为82M-86M,不是时钟信号。

是否有工程师碰到过类似的问题?现在怀疑和LVDS信号本身有关,如果925不工作,无任何发射,928不工作,会有一些幅值,因此可能大多数和925有关,与板上的其它芯片没有太大关系。86M与LVDS信号频率1.8G相比比较低,因此怀疑可能为调制在上面的I2C(约400K)有关,放大超标点,确实有间隔约350-400K的频点。

基于以上分析,想去LVDS信号处理,但高频信号不好处理。想请教TI的各位工程师,是否我的分析有误,或者有什么好的方法来解决此问题,其它LVDS IC也有类似问题的案例吗?