This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCF5801A

可编程延迟和相位控制中,在DLYCTR引脚的第32个上升沿上,在接下来的一次或者两次DLYCTR引脚的上升沿中,不会更新相位。能否解答一下到底是一次还是两次?

  • Hi,

    DATA sheet 中描述:For every 32 edges, there are one or two edges for which the phase aligner does not update the phase.

    它可并没有说是one or two rising edge哦?! 明白了吧,就是说会有下降沿,当然那个是“附带的”。

  • 您好,在DATA sheet中Table 3. Programmable Delay and Phase Alignment第一列的确说的是每一个DLYCTR的上升沿。另外,还有一个问题,DLYCTRL引脚的频率一定要小于或者等于LEADLAG引脚的频率吗?LEADLAG引脚只是控制信号,频率很低然而DLYCTRL引脚可以很高啊

  • 您好,在DATA sheet中Table 3. Programmable Delay and Phase Alignment第一列的确说的是每一个DLYCTR的上升沿。另外,还有一个问题,DLYCTRL引脚的频率一定要小于或者等于LEADLAG引脚的频率吗?LEADLAG引脚只是控制信号,频率很低然而DLYCTRL引脚可以很高啊

x 出现错误。请重试或与管理员联系。