This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

iso5500这个芯片是不是有问题?

Other Parts Discussed in Thread: ISO5500EVM

我在用ISO5500开发板的时候,用两块ISO500开发板做半桥驱动,我发现在上桥臂的IGBT的D端和S端的电压很大,在图中就是Q1的D和S端的电压很大,v+和v-是320的电压,而OUT-T1的输出电压只是在0V到25V的方波,不知道为什么?请大侠们解释下。

图中的R17和R20都没有,就是短路线短接的。ISO5500的15V供电电压的地是和V-连接的,否则ISO5500的G端没有波形。