大家好,我现在的电路中有3v和5v的供电,其中用到了3v器件和5v供电器件之间的总线通信(SPI)和时钟信号的输入输出等。因此,我打算采用集成逻辑电平转换芯片。我知道数字电路中,门电路的驱动是要考虑扇入扇出的,我现在不清楚是否要考虑电平转换芯片的驱动能力,如果考虑该如何考虑?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,我现在的电路中有3v和5v的供电,其中用到了3v器件和5v供电器件之间的总线通信(SPI)和时钟信号的输入输出等。因此,我打算采用集成逻辑电平转换芯片。我知道数字电路中,门电路的驱动是要考虑扇入扇出的,我现在不清楚是否要考虑电平转换芯片的驱动能力,如果考虑该如何考虑?
可以考虑SN74AVC4T774这款可用于SPI总线电平转换,驱动能力可参考数据手册中的Iol和Ioh这两个值。
您好,我的电路中是一个5v供电的DAC 和一个3,3v供电的msp430 我目前最关心的是在选择电平转换芯片的时候是否要考虑电压转换芯片的驱动能力。我了解到,现在大部分都是cmos工艺,是电压控制的,所需的电流是非常低的。因此两个cmos器件之间的电压转换是否还要考虑电压转换芯片的驱动能力。谢谢!
是的,一般所需的电流都很小,像你的应用中,比如5V~3.3V转换,需要看下430 IO口所需输入电流的大小从而判断电平转换是否能够驱动。TI有两类电平转换,一类是自动方向控制的TXS和TXB系列的电平转换,输出电流大小是和供电电压有关系的,还有一类就是上面提到带方向控制位的SN74系列的,输出电流可参考datashet中Iol和Ioh这两个参数。
您好:麻烦推荐一款替代sn74avc4t774的逻辑总线电平转换芯片(5V供电),我是输入3.3v(来自ARM)转输出5V,5V端驱动SPI接口(DAC8311)。