手册上说有两种配置方法,一种是硬件,一种是I2C,是不是两种配置都可以实现12bit模式?还有就是硬件配置时置高置低时是不是接电源VDD为置高接地为置低?不一定用接到FPGA引脚上吧
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
手册上说有两种配置方法,一种是硬件,一种是I2C,是不是两种配置都可以实现12bit模式?还有就是硬件配置时置高置低时是不是接电源VDD为置高接地为置低?不一定用接到FPGA引脚上吧
12bit或24bit是通过引脚BSEL的高低电平来决定的,当BSEL=H,为24bit模式,当BSEL=L,为12bit模式。 两种配置都可以实现12bit模式。
还有一个问题,24bit模式就是时钟的上升或下降沿进行锁存数据,12bit模式就是时钟上升沿和下降沿都在锁存数据吧?走相同数目的时钟这两种模式传输的数据位是相同的?谢谢
12bit是时钟的上升沿和下降沿都锁存数据,同样数目的时钟,根据datasheet page13 的data mapping来看传输的数据位数是相同的,都是RGB888模式。
我看datasheet上面有一个参考电压VREF,用来选择low-swing和high-swing模式,这是什么意思?谢谢
图形控制接口有这两种模式,high-swing模式指的是3.3V接口电平, 而low-swing模式指的是1.1V~1.8V接口电平。
我看datasheet里有个function图,里面有个I2C for DDC,这是做什么的呢?我看dvi接口也有ddc管脚,这是要连上吗
DDC 指的是Display Data Channel。指的是发送和接收通过DDC这个通道知道彼此的发送和接收的情况。 DVI接口中,5V DDC引脚是要接上的。