大家好,我是个菜鸟,请问大家有没有使用过TUSB2046BI,这个芯片是1转4的USB-HUB,但是它的数据手册上写的是3.3V--3.6V供电,感觉这个不太主流啊,用LM2853输出的3.3V供电可以吗?
最低要求是3.3V,我的电源系统里只有3.3V,是不是不可以用这个芯片啊?板子是工业级的,不能用TUSB2046B,只能用TUSB2046BI,求大神赐教。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kailyn Chen,感谢您能回答我的问题,但是做实验时(静电,射频传导,浪涌等)会不会对3.3v产生影响,导致3.3V波动,USB是不是就不能正常工作了?
一开始还是想过用3.3V的,但是害怕不严谨,板子出来了试验不通过就会造成很大的损失,您能确定这个用3.3V是没问题的吗?多谢!
实验时还是需要注意静电,射频传导对器件造成的影响。
另外,对于工作电压的问题,最低为3.3V,最高为3.6V,在这个范围内都是能够正常工作的(包括最低和最高电压),但需要注意的是你使用LM2853的输出来给供电,输出精度的问题,比如说是3.2xxxV~3.3xxxV范围内,那么就很难保证TUSB2046BI的性能了。 总的来说,TUSB2046BI的供电不能低于3.3V。