This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385的一个usb0做gadget 模式。 usb1做host 模式



我按照ti的TI81XX_PSP_USB_Configuration_Guide手册去配置One port as host and other port as Gadget 。

启动开发板后。我做如下步骤

1. insmod g_ether.ko (usb0 port will be enabled as cdc/rndis gadget)
2. insmod g_zero.ko (usb1 port will enabled as host mode and all devices (eg.USB-HDD/flash drive etc) connected
to this port will be enumerated
3. rmmod g_ether.ko (remove the gadget driver from usb0 port)
4. insmod g_file_storage.ko file=/dev/sda stall=0 buflen=65536 (or use g_mass_storage.ko)
Now the usb0 port can be connected to window/linux host as mass storage gadget with USB-HDD (/dev/sda) as
storage media.

 在usb1插入U盘没有反应

usb0用usb标准电缆连接ps,也没有反应

谁知道怎么回事