This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MCU使用的是STM32F103C8T6,CAN使用的ISO1050,在调试的过程中,ISO1050始终不通,电源这些都检查了,3.3V纹波在100MV作用,电源都算正常。发现TX,RX波形不对,
TX波形:
亲;建议查一下管脚有没有虚焊或者换片新的。建议焊新IC时;拔掉烙铁电源。
现在能够通信了,只是波特率高于125K就不能通信,不知道为什么。
125Kbps应该是没有问题的,因为ISO1050能够支持到1Mbps。只是对最低data rate有要求不能低于37Kbps。
你好,为什么我设计的只能跑125K以下,125K以上波特率是不是与采样率有关系?
您用的ISO1050,用一个电源隔离降压模块去提供5V的隔离后的电,功耗会很大吗?